Other Parts Discussed in Thread: MSP430F5438, MSP430G2553
Hello all,
I am currently migrating code from an existing non-microcontroller project into the MSP430 framework targeting a MSP430F5438 through CCSv . The legacy code makes use of a lot of global variables which are placed in the .bss section. Unfortunately, the total size of the resulting .bss section is 21kb (0x5744) and the F5438 is only 16kb (0x4000).
When modifying the default lnk_msp430f5438.cmb linker command file to place the large .bss section in Flash (see below) and then launching in debug mode, the micro hangs and wanders through memory aimlessly indicated when halting the processor the resulting PC is up in the FLASH2 memory address space (e.g. 0x1A190).
Modification to linker command file:
Changed:
.bss : {} > RAM /* GLOBAL & STATIC VARS */
to:
.bss : {} > FLASH /* GLOBAL & STATIC VARS */
Furthermore, I have enabled: --code_model=large --data_model=large --near_data=none and silicon version mspx to support the >64kb memory space. The contents of the resulting map file is below. The entry point seems to make sense falling within the .text:_isr section; however, the processor seems to get lost after that.
Are there specific sections of .bss that need to remain in RAM or should be loaded into RAM at run-time to ensure proper operation? If so, any advice on how to achieve this? RAM is now rather empty using only 0x00a0 so I can afford to place any portions of the .bss section in there through the linker command file. I'm thinking the following but wanted to confirm if that was true and in fact how to do it:
rts430x.lib : _lock.obj (.bss) and rts430x.lib: boot.obj (.bss)
When following the instructions from slau131e section 7.5.4.5 Specifying Library or Archive Members as Input to Output Sections in the following manner I receive the errors below:
Further modification to linker command file:
Changed:
.bss : {} > FLASH /* GLOBAL & STATIC VARS */
to:
.bss > RAM
{
main.obj (.bss)
-l=rts430xl.lib<boot.obj> (.bss)
-l=rts430xl.lib<_lock.obj> (.bss)
}
.bss > FLASH
{
* (.bss)
}
Errors generated:
"../lnk_msp430f5438.cmd", line 108: error: -l must specify a filename
"../lnk_msp430f5438.cmd", line 108: error: cannot find file "boot.obj"
"../lnk_msp430f5438.cmd", line 108: error: cannot find file ".bss"
"../lnk_msp430f5438.cmd", line 109: error: cannot find file "_lock.obj"
"../lnk_msp430f5438.cmd", line 109: error: cannot find file ".bss"
Any insights anyone might have would be great!
Thanks very much,
- Mark
******************************************************************************
MSP430 Linker PC v3.3.0
******************************************************************************
>> Linked Thu Nov 11 10:30:02 2010
OUTPUT FILE NAME: <FREDI.out>
ENTRY POINT SYMBOL: "_c_int00" address: 0000db3c
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
SFR 00000000 00000010 00000000 00000010 RWIX
PERIPHERALS_8BIT 00000010 000000f0 00000000 000000f0 RWIX
PERIPHERALS_16BIT 00000100 00000100 00000000 00000100 RWIX
INFOD 00001800 00000080 00000000 00000080 RWIX
INFOC 00001880 00000080 00000000 00000080 RWIX
INFOB 00001900 00000080 00000000 00000080 RWIX
INFOA 00001980 00000080 00000000 00000080 RWIX
RAM 00001c00 00004000 000000a0 00003f60 RWIX
FLASH 00005c00 0000a380 0000a380 00000000 RWIX
INT00 0000ff80 00000002 00000000 00000002 RWIX
INT01 0000ff82 00000002 00000000 00000002 RWIX
INT02 0000ff84 00000002 00000000 00000002 RWIX
INT03 0000ff86 00000002 00000000 00000002 RWIX
INT04 0000ff88 00000002 00000000 00000002 RWIX
INT05 0000ff8a 00000002 00000000 00000002 RWIX
INT06 0000ff8c 00000002 00000000 00000002 RWIX
INT07 0000ff8e 00000002 00000000 00000002 RWIX
INT08 0000ff90 00000002 00000000 00000002 RWIX
INT09 0000ff92 00000002 00000000 00000002 RWIX
INT10 0000ff94 00000002 00000000 00000002 RWIX
INT11 0000ff96 00000002 00000000 00000002 RWIX
INT12 0000ff98 00000002 00000000 00000002 RWIX
INT13 0000ff9a 00000002 00000000 00000002 RWIX
INT14 0000ff9c 00000002 00000000 00000002 RWIX
INT15 0000ff9e 00000002 00000000 00000002 RWIX
INT16 0000ffa0 00000002 00000000 00000002 RWIX
INT17 0000ffa2 00000002 00000000 00000002 RWIX
INT18 0000ffa4 00000002 00000000 00000002 RWIX
INT19 0000ffa6 00000002 00000000 00000002 RWIX
INT20 0000ffa8 00000002 00000000 00000002 RWIX
INT21 0000ffaa 00000002 00000000 00000002 RWIX
INT22 0000ffac 00000002 00000000 00000002 RWIX
INT23 0000ffae 00000002 00000000 00000002 RWIX
INT24 0000ffb0 00000002 00000000 00000002 RWIX
INT25 0000ffb2 00000002 00000000 00000002 RWIX
INT26 0000ffb4 00000002 00000000 00000002 RWIX
INT27 0000ffb6 00000002 00000000 00000002 RWIX
INT28 0000ffb8 00000002 00000000 00000002 RWIX
INT29 0000ffba 00000002 00000000 00000002 RWIX
INT30 0000ffbc 00000002 00000000 00000002 RWIX
INT31 0000ffbe 00000002 00000000 00000002 RWIX
INT32 0000ffc0 00000002 00000000 00000002 RWIX
INT33 0000ffc2 00000002 00000000 00000002 RWIX
INT34 0000ffc4 00000002 00000000 00000002 RWIX
INT35 0000ffc6 00000002 00000000 00000002 RWIX
INT36 0000ffc8 00000002 00000000 00000002 RWIX
INT37 0000ffca 00000002 00000000 00000002 RWIX
INT38 0000ffcc 00000002 00000000 00000002 RWIX
INT39 0000ffce 00000002 00000000 00000002 RWIX
INT40 0000ffd0 00000002 00000000 00000002 RWIX
INT41 0000ffd2 00000002 00000000 00000002 RWIX
INT42 0000ffd4 00000002 00000000 00000002 RWIX
INT43 0000ffd6 00000002 00000000 00000002 RWIX
INT44 0000ffd8 00000002 00000002 00000000 RWIX
INT45 0000ffda 00000002 00000000 00000002 RWIX
INT46 0000ffdc 00000002 00000002 00000000 RWIX
INT47 0000ffde 00000002 00000000 00000002 RWIX
INT48 0000ffe0 00000002 00000000 00000002 RWIX
INT49 0000ffe2 00000002 00000002 00000000 RWIX
INT50 0000ffe4 00000002 00000000 00000002 RWIX
INT51 0000ffe6 00000002 00000000 00000002 RWIX
INT52 0000ffe8 00000002 00000000 00000002 RWIX
INT53 0000ffea 00000002 00000000 00000002 RWIX
INT54 0000ffec 00000002 00000000 00000002 RWIX
INT55 0000ffee 00000002 00000000 00000002 RWIX
INT56 0000fff0 00000002 00000000 00000002 RWIX
INT57 0000fff2 00000002 00000000 00000002 RWIX
INT58 0000fff4 00000002 00000000 00000002 RWIX
INT59 0000fff6 00000002 00000000 00000002 RWIX
INT60 0000fff8 00000002 00000000 00000002 RWIX
INT61 0000fffa 00000002 00000000 00000002 RWIX
INT62 0000fffc 00000002 00000000 00000002 RWIX
RESET 0000fffe 00000002 00000002 00000000 RWIX
FLASH2 00010000 00035c00 0000a5fd 0002b603 RWIX
SECTION ALLOCATION MAP
output attributes/
section page origin length input sections
-------- ---- ---------- ---------- ----------------
.pinit 0 00005c00 00000000 UNINITIALIZED
.stack 0 00005b60 000000a0 UNINITIALIZED
00005b60 00000004 rts430xl.lib : boot.obj (.stack)
00005b64 0000009c --HOLE--
.bss 0 00005c00 00005748 UNINITIALIZED
00005c00 00001060 sri_quart.obj (.bss)
00006c60 00000e70 sri_frwv_cmd_packet_selftest.obj (.bss)
00007ad0 00000dce sri_frwv_send_selftest.obj (.bss)
0000889e 00000896 sri_frwv_cmd_fill_frames_selftest.obj (.bss)
00009134 000004ca main.obj (.bss)
000095fe 000003a6 sri_m2k_send_selftest.obj (.bss)
000099a4 00000344 sri_frwv_cmd_packet.obj (.bss)
00009ce8 0000033e sri_pparse_cntxts.obj (.bss)
0000a026 00000330 sri_frwv_packet_selftest.obj (.bss)
0000a356 00000310 sri_test_harness.obj (.bss)
0000a666 000002ca sri_m2k_msg_selftest.obj (.bss)
0000a930 00000240 sri_frwv_dual_parse_selftest.obj (.bss)
0000ab70 000001a4 sri_frwv_ack_selftest.obj (.bss)
0000ad14 000000d2 fredi_imls.obj (.bss)
0000ade6 000000cf fredi_m2k.obj (.bss)
0000aeb5 00000001 sri_frwv_dual_parse.obj (.bss)
0000aeb6 000000c4 sri_frwv_cmd_fill_selftest.obj (.bss)
0000af7a 000000c2 sri_m2k_display.obj (.bss)
0000b03c 0000006a sri_m2k_msg.obj (.bss)
0000b0a6 00000068 sri_frwv_cmd_packet_epoch_selftest.obj (.bss)
0000b10e 00000060 sri_ubx_binary_msg.obj (.bss)
0000b16e 0000005c sri_rtca_data.obj (.bss)
0000b1ca 00000042 sri_tspi_data.obj (.bss)
0000b20c 00000039 sri_imiles_msg.obj (.bss)
0000b245 00000001 sri_m2k_spoof.obj (.bss)
0000b246 00000030 sri_msgqueue_selftest.obj (.bss)
0000b276 0000002c fredi_frwv.obj (.bss)
0000b2a2 00000017 sri_frwv_ack.obj (.bss)
0000b2b9 00000001 --HOLE--
0000b2ba 00000015 sri_frwv_packet.obj (.bss)
0000b2cf 00000001 --HOLE--
0000b2d0 00000014 fredi_stats.obj (.bss)
0000b2e4 00000014 sri_imiles_send.obj (.bss)
0000b2f8 00000014 sri_time.obj (.bss)
0000b30c 0000000e sri_m2k_send.obj (.bss)
0000b31a 00000008 rts430xl.lib : _lock.obj (.bss)
0000b322 00000008 : boot.obj (.bss)
0000b32a 00000008 sri_frwv_send_fill.obj (.bss)
0000b332 00000007 fredi_frwv_status.obj (.bss)
0000b339 00000001 --HOLE--
0000b33a 00000005 sri_frwv_cmd_fill.obj (.bss)
0000b33f 00000001 --HOLE--
0000b340 00000004 fredi_uart.obj (.bss)
0000b344 00000002 sri_debug.obj (.bss)
0000b346 00000002 sri_hardware_status.obj (.bss)
.cinit 0 0000b348 0000279c
0000b348 00000dda sri_frwv_send_selftest.obj (.cinit)
0000c122 00000788 sri_frwv_cmd_fill_frames_selftest.obj (.cinit)
0000c8aa 00000430 sri_frwv_cmd_packet_selftest.obj (.cinit)
0000ccda 00000294 sri_frwv_packet_selftest.obj (.cinit)
0000cf6e 000001be sri_frwv_dual_parse_selftest.obj (.cinit)
0000d12c 0000018c sri_frwv_ack_selftest.obj (.cinit)
0000d2b8 0000017e sri_m2k_msg_selftest.obj (.cinit)
0000d436 0000017c sri_m2k_send_selftest.obj (.cinit)
0000d5b2 000000c6 sri_frwv_cmd_fill_selftest.obj (.cinit)
0000d678 000000a8 sri_m2k_display.obj (.cinit)
0000d720 00000096 sri_pparse_cntxts.obj (.cinit)
0000d7b6 00000074 sri_frwv_cmd_packet_epoch_selftest.obj (.cinit)
0000d82a 00000064 sri_m2k_msg.obj (.cinit)
0000d88e 00000054 fredi_imls.obj (.cinit)
0000d8e2 00000045 sri_imiles_msg.obj (.cinit)
0000d927 00000001 --HOLE-- [fill = 0]
0000d928 00000043 fredi_m2k.obj (.cinit)
0000d96b 00000001 --HOLE-- [fill = 0]
0000d96c 00000041 sri_msgqueue_selftest.obj (.cinit)
0000d9ad 00000001 --HOLE-- [fill = 0]
0000d9ae 00000040 sri_rtca_data.obj (.cinit)
0000d9ee 00000021 sri_frwv_packet.obj (.cinit)
0000da0f 00000001 --HOLE-- [fill = 0]
0000da10 00000020 sri_frwv_send_fill.obj (.cinit)
0000da30 0000001e sri_ubx_binary_msg.obj (.cinit)
0000da4e 00000017 fredi_frwv_status.obj (.cinit)
0000da65 00000001 --HOLE-- [fill = 0]
0000da66 00000011 sri_frwv_cmd_fill.obj (.cinit)
0000da77 00000001 --HOLE-- [fill = 0]
0000da78 0000000f fredi_frwv.obj (.cinit)
0000da87 00000001 --HOLE-- [fill = 0]
0000da88 0000000f main.obj (.cinit)
0000da97 00000001 --HOLE-- [fill = 0]
0000da98 0000000f sri_debug.obj (.cinit)
0000daa7 00000001 --HOLE-- [fill = 0]
0000daa8 0000000a fredi_stats.obj (.cinit)
0000dab2 00000008 sri_test_harness.obj (.cinit)
0000daba 00000007 sri_frwv_ack.obj (.cinit)
0000dac1 00000001 --HOLE-- [fill = 0]
0000dac2 00000007 sri_frwv_cmd_packet.obj (.cinit)
0000dac9 00000001 --HOLE-- [fill = 0]
0000daca 00000007 sri_frwv_dual_parse.obj (.cinit)
0000dad1 00000001 --HOLE-- [fill = 0]
0000dad2 00000007 sri_imiles_send.obj (.cinit)
0000dad9 00000001 --HOLE-- [fill = 0]
0000dada 00000007 sri_m2k_spoof.obj (.cinit)
0000dae1 00000001 --HOLE-- [fill = 0]
0000dae2 00000002 (.pad.cinit) [fill = 0]
.text:_isr
* 0 0000dae4 000000aa
0000dae4 00000058 sri_quart.obj (.text:_isr:USCI_A1_ISR)
0000db3c 0000002a rts430xl.lib : boot.obj (.text:_isr:_c_int00_noexit)
0000db66 0000001a sri_quart.obj (.text:_isr:USCI_A3_ISR)
0000db80 0000000e sri_time.obj (.text:_isr:TIMER1_A0_ISR)
.text.1 0 0000db8e 000023f2
0000db8e 00000a2c sri_frwv_cmd_packet.obj (.text:sri_frwv_cmd_packet_dispatch)
0000e5ba 000008f0 sri_ubx_binary_msg.obj (.text:sri_ubx_bmsg_dispatch)
0000eeaa 000006ba sri_m2k_msg.obj (.text:sri_m2k_msg_dispatch)
0000f564 000004da sri_pparse.obj (.text:sri_pparse)
0000fa3e 0000041a sri_frwv_packet.obj (.text:sri_frwv_packet_dispatch)
0000fe58 00000128 sri_frwv_packet.obj (.text:sri_frwv_do_frequency_cmd)
.int44 0 0000ffd8 00000002
0000ffd8 00000002 sri_quart.obj (.int44)
.int46 0 0000ffdc 00000002
0000ffdc 00000002 sri_quart.obj (.int46)
.int49 0 0000ffe2 00000002
0000ffe2 00000002 sri_time.obj (.int49)
.reset 0 0000fffe 00000002
0000fffe 00000002 rts430xl.lib : boot.obj (.reset)
.const 0 00010000 0000391f
00010000 00000a34 sri_frwv_cmd_packet.obj (.const:.string)
00010a34 000006e6 sri_frwv_packet.obj (.const:.string)
0001111a 000003b4 sri_m2k_msg.obj (.const:.string)
000114ce 00000334 sri_frwv_send_selftest.obj (.const:.string)
00011802 00000218 sri_m2k_display.obj (.const:.string)
00011a1a 00000200 sri_test_harness.obj (.const:.string)
00011c1a 000001ae sri_tspi_data.obj (.const:.string)
00011dc8 000001a6 fredi_m2k.obj (.const:.string)
00011f6e 000001a4 fredi_imls.obj (.const:.string)
00012112 0000019a sri_debug.obj (.const:.string)
000122ac 00000194 sri_frwv_send_fill.obj (.const:.string)
00012440 00000186 sri_msgqueue_selftest.obj (.const:.string)
000125c6 00000168 sri_frwv_cmd_packet_epoch_selftest.obj (.const:.string)
0001272e 00000160 sri_frwv_cmd_fill_frames_selftest.obj (.const:.string)
0001288e 00000152 sri_m2k_msg_selftest.obj (.const:.string)
000129e0 00000150 sri_rtca_data.obj (.const:.string)
00012b30 00000144 sri_frwv_cmd_packet_selftest.obj (.const:.string)
00012c74 00000136 sri_frwv_packet_selftest.obj (.const:.string)
00012daa 000000fa sri_frwv_ack.obj (.const:.string)
00012ea4 000000f8 sri_frwv_dual_parse_selftest.obj (.const:.string)
00012f9c 000000f4 sri_ubx_binary_msg.obj (.const:.string)
00013090 000000ee sri_m2k_send_selftest.obj (.const:.string)
0001317e 000000e0 sri_frwv_cmd_fill_selftest.obj (.const:.string)
0001325e 000000d8 sri_frwv_ack_selftest.obj (.const:.string)
00013336 000000aa sri_imiles_msg.obj (.const:.string)
000133e0 0000009c fredi_frwv_data.obj (.const:.string)
0001347c 0000009c sri_m2k_spoof.obj (.const:.string)
00013518 00000062 fredi_stats.obj (.const:.string)
0001357a 00000062 sri_msgqueue.obj (.const:.string)
000135dc 00000060 fredi_qhandlers.obj (.const:.string)
0001363c 0000005e sri_frwv_cmd_fill.obj (.const:.string)
0001369a 0000005e sri_pparse_cntxts.obj (.const:sri_m2k_lens)
000136f8 00000052 fredi_frwv_status.obj (.const:.string)
0001374a 00000040 sri_hardware_status.obj (.const:.string)
0001378a 00000034 fredi_frwv.obj (.const:.string)
000137be 0000002c sri_time.obj (.const:.string)
000137ea 0000002a fredi_les.obj (.const:.string)
00013814 0000002a sri_frwv_dual_parse.obj (.const:.string)
0001383e 00000024 sri_imiles_send.obj (.const:.string)
00013862 0000001e sri_m2k_send.obj (.const:.string)
00013880 0000001e sri_queue.obj (.const:.string)
0001389e 0000001c sri_quart.obj (.const:.string)
000138ba 0000001c sri_m2k_display.obj (.const)
000138d6 00000018 main.obj (.const:.string)
000138ee 00000016 sri_pparse.obj (.const:.string)
00013904 00000014 rts430xl.lib : _printfi_min.obj (.const:.string)
00013918 00000002 sri_pparse_cntxts.obj (.const:sri_Imiles_sync)
0001391a 00000002 sri_pparse_cntxts.obj (.const:sri_m2k_sync)
0001391c 00000002 sri_pparse_cntxts.obj (.const:sri_ubx_sync)
0001391e 00000001 sri_pparse_cntxts.obj (.const:sri_frwv_sync)
.text.2 0 00013920 00006cde
00013920 00000410 sri_msgqueue_selftest.obj (.text:test_msgq_basic)
00013d30 000003a2 sri_frwv_packet.obj (.text:sri_frwv_packet_dispatch_edi_cmd)
000140d2 000002d6 sri_frwv_send_fill.obj (.text:sri_frwv_fill_PDU_tspi)
000143a8 00000200 sri_frwv_send_selftest.obj (.text:packet_run_test)
000145a8 000001f4 sri_frwv_packet.obj (.text:DoSlotCmd)
0001479c 000001f2 sri_frwv_packet.obj (.text:DoDamageCmdM2k)
0001498e 000001d6 sri_frwv_cmd_packet_selftest.obj (.text:frwv_cmd_cmp_cmd_data)
00014b64 000001ce sri_frwv_send_fill.obj (.text:sri_frwv_translate_damage)
00014d32 000001bc sri_frwv_packet.obj (.text:DoDamageCmdImls)
00014eee 000001ba sri_frwv_dual_parse.obj (.text:sri_frwv_dual_parse)
000150a8 000001b8 sri_m2k_msg_selftest.obj (.text:m2kmsg_run_test)
00015260 000001b2 sri_m2k_send_selftest.obj (.text:m2k_send_run_test)
00015412 000001ae sri_frwv_cmd_fill.obj (.text:sri_frwv_cmd_request_set_RAM_frametable_internal)
000155c0 00000184 sri_frwv_send_fill.obj (.text:sri_frwv_fill_slave_PDU)
00015744 00000182 sri_frwv_cmd_fill_selftest.obj (.text:cmd_fill_run_test)
000158c6 00000182 sri_frwv_cmd_packet_epoch_selftest.obj (.text:cmd_packet_epoch_run_test)
00015a48 00000180 rts430xl.lib : _printfi_min.obj (.text:_setfield)
00015bc8 0000017e sri_frwv_cmd_fill.obj (.text:sri_frwv_cmd_fill_SuperEpoch)
00015d46 00000178 sri_frwv_ack_selftest.obj (.text:ack_run_test)
00015ebe 00000174 sri_frwv_cmd_packet.obj (.text:sri_frwv_cmd_data_calc_push_delay_ticks)
00016032 00000160 sri_frwv_dual_parse_selftest.obj (.text:dparse_run_test)
00016192 00000160 main.obj (.text:main)
000162f2 00000156 sri_frwv_packet.obj (.text:sri_frwv_do_super_epoch_cmd)
00016448 0000014c sri_frwv_cmd_fill_frames_selftest.obj (.text:cmd_fill_frames_run_test)
00016594 0000014c sri_frwv_cmd_packet_selftest.obj (.text:cmd_packet_run_test)
000166e0 00000140 sri_test_harness.obj (.text:sri_test_harness_cmp_bytes)
00016820 00000132 sri_frwv_cmd_fill.obj (.text:sri_frwv_cmd_fill_READ_BULK)
00016952 00000132 sri_frwv_packet.obj (.text:sri_frwv_packet_dispatch_cmd_size)
00016a84 00000130 sri_frwv_send_fill.obj (.text:sri_frwv_fill_dump_struct)
00016bb4 00000126 sri_rtca_data.obj (.text:sri_rtca_data_describe_damage)
00016cda 0000011c sri_frwv_ack.obj (.text:sri_frwv_ack_enqueue)
00016df6 0000011a sri_m2k_spoof.obj (.text:sri_m2k_spoof_vest)
00016f10 00000118 sri_frwv_cmd_fill.obj (.text:sri_frwv_cmd_fill_slot_buffer)
00017028 00000110 sri_frwv_send_fill.obj (.text:sri_frwv_fill_PDU_hw)
00017138 00000100 sri_frwv_send_fill.obj (.text:sri_frwv_fill_slave_packet)
00017238 000000f8 sri_m2k_send.obj (.text:sri_m2k_send_ack)
00017330 000000f2 sri_m2k_msg_selftest.obj (.text:m2kmsg_cmp_rtca_rte_data)
00017422 000000ee sri_frwv_cmd_packet.obj (.text:sri_frwv_cmd_data_init)
00017510 000000ec sri_frwv_cmd_packet.obj (.text:addDispatchEntry)
000175fc 000000ea sri_frwv_cmd_packet.obj (.text:sri_frwv_cmd_data_calc_epoch_us)
000176e6 000000e4 sri_frwv_send_fill.obj (.text:sri_frwv_fill_prepare_pdu)
000177ca 000000e4 sri_tspi_data.obj (.text:sri_tspi_debug_dump_utc_time)
000178ae 000000de sri_frwv_packet_selftest.obj (.text:packet_run_test)
0001798c 000000d6 rts430xl.lib : _printfi_min.obj (.text:_printfi_minimal)
00017a62 000000d6 sri_frwv_cmd_fill.obj (.text:sri_frwv_cmd_fill_EEPROM_READ_WRITE)
00017b38 000000d4 sri_rtca_data.obj (.text:sri_rtca_rte_debug_dump)
00017c0c 000000ce sri_frwv_cmd_fill.obj (.text:sri_frwv_cmd_request_buffer)
00017cda 000000c8 sri_frwv_cmd_fill.obj (.text:sri_frwv_cmd_fill_WRITE_RAM_TDMA)
00017da2 000000c8 sri_m2k_send.obj (.text:sri_m2k_send_setpid)
00017e6a 000000c4 sri_queue.obj (.text:sri_queue_write)
00017f2e 000000c0 sri_m2k_display.obj (.text:lot2Line2Formatter)
00017fee 000000ba sri_queue.obj (.text:sri_queue_read)
000180a8 000000ba sri_tspi_data.obj (.text:sri_tspi_debug_dump_space)
00018162 000000b6 sri_tspi_data.obj (.text:sri_tspi_debug_dump_gps_time)
00018218 000000b4 sri_frwv_cmd_fill.obj (.text:sri_frwv_cmd_fill_internal)
000182cc 000000b4 sri_frwv_cmd_packet.obj (.text:sri_frwv_cmd_packet_check_tdma_values)
00018380 000000aa fredi_qhandlers.obj (.text:_fredi_qhandlers_parse_generic)
0001842a 0000009c sri_frwv_ack.obj (.text:sri_frwv_ack_dequeue)
000184c6 0000009c sri_m2k_msg.obj (.text:sri_m2k_msg_decode_pid)
00018562 0000009c sri_m2k_send.obj (.text:sri_m2k_send_admin_kill)
000185fe 0000009c sri_m2k_send.obj (.text:sri_m2k_send_rte)
0001869a 00000094 sri_frwv_cmd_packet.obj (.text:sri_frwv_cmd_packet_check_id_values)
0001872e 00000092 fredi_qhandlers.obj (.text:_fredi_qhandlers_fill_buf)
000187c0 00000092 sri_frwv_cmd_packet.obj (.text:sri_frwv_cmd_data_calc_numUsedFrames)
00018852 00000092 fredi_frwv.obj (.text:sri_frwv_xmit)
000188e4 0000008c rts430xl.lib : _printfi_min.obj (.text:_ltostr)
00018970 0000008a sri_frwv_cmd_packet.obj (.text:sri_frwv_cmd_packet_were_slots_set)
000189fa 00000088 sri_frwv_send_fill.obj (.text:sri_frwv_fill_PDU_m2k)
00018a82 00000086 sri_frwv_cmd_packet.obj (.text:sri_frwv_freq_data_set)
00018b08 00000084 sri_msgqueue.obj (.text:sri_msgqueue_dequeue)
00018b8c 00000084 sri_msgqueue.obj (.text:sri_msgqueue_enqueue)
00018c10 00000080 sri_frwv_send_fill.obj (.text:sri_frwv_fill_PDU_tess)
00018c90 0000007c sri_m2k_msg.obj (.text:m2k_xmit_setpid)
00018d0c 00000078 sri_frwv_cmd_packet.obj (.text:sri_frwv_cmd_packet_is_epoch_valid)
00018d84 00000076 sri_msgqueue.obj (.text:sri_msgqueue_init)
00018dfa 00000070 rts430xl.lib : vsnprintf.obj (.text:vsnprintf)
00018e6a 0000006e sri_m2k_send.obj (.text:sri_m2k_send_dpcutype)
00018ed8 0000006e sri_m2k_send.obj (.text:sri_m2k_send_reset)
00018f46 0000006e sri_m2k_send.obj (.text:sri_m2k_send_resurrect)
00018fb4 0000006e sri_m2k_send.obj (.text:sri_m2k_send_status)
00019022 0000006e sri_queue.obj (.text:sri_queue_enqueue)
00019090 0000006c fredi_uart.obj (.text:UART_putChar)
000190fc 0000006c rts430xl.lib : vsnprintf.obj (.text:_outs)
00019168 0000006c sri_frwv_packet.obj (.text:compare_radio_info)
000191d4 00000066 sri_imiles_send.obj (.text:sri_imls_send_admin_kill)
0001923a 00000066 sri_queue.obj (.text:sri_queue_dequeue)
000192a0 00000062 sri_pparse.obj (.text:sri_pparse_client_done)
00019302 00000060 rts430xl.lib : _printfi_min.obj (.text:_getarg_diouxp)
00019362 00000060 sri_quart.obj (.text:quart_init)
000193c2 00000060 sri_pparse.obj (.text:sri_pparse_init)
00019422 00000060 sri_queue.obj (.text:sri_queue_init)
00019482 0000005c rts430xl.lib : autoinit.obj (.text:_auto_init)
000194de 0000005a : _printfi_min.obj (.text:_pproc_diouxp)
00019538 0000005a sri_imiles_send.obj (.text:sri_imls_send_reset)
00019592 0000005a sri_time.obj (.text:time_init)
000195ec 00000058 sri_m2k_display.obj (.text:lot2Line1Formatter)
00019644 00000058 rts430xl.lib : div32u.obj (.text)
0001969c 00000058 sri_pparse.obj (.text:sri_pparse_is_parser_reset)
000196f4 00000058 sri_time.obj (.text:time_now)
0001974c 00000056 sri_frwv_ack.obj (.text:sri_frwv_ack_init)
000197a2 00000054 sri_m2k_msg_selftest.obj (.text:m2kmsg_cmp_rtca_static_data)
000197f6 00000054 sri_frwv_packet.obj (.text:reset_radio_info)
0001984a 00000052 fredi_uart.obj (.text:UART_printf)
0001989c 00000050 fredi_io.obj (.text:init_MM2_uart)
000198ec 00000048 rts430xl.lib : _printfi_min.obj (.text:_pproc_str)
00019934 00000048 sri_rtca_data.obj (.text:sri_rtca_data_init)
0001997c 00000046 sri_quart.obj (.text:quart_read)
000199c2 00000046 sri_quart.obj (.text:quart_write)
00019a08 00000044 fredi_uart.obj (.text:UART_write)
00019a4c 00000044 rts430xl.lib : sprintf.obj (.text:sprintf)
00019a90 00000044 sri_pparse.obj (.text:sri_pparse_is_payload_valid)
00019ad4 00000042 fredi_frwv_status.obj (.text:sri_freewave_status_debug)
00019b16 00000042 sri_frwv_send_fill.obj (.text:sri_frwv_fill_init)
00019b58 00000042 sri_m2k_display.obj (.text:sri_m2k_display_set_rit_init)
00019b9a 00000040 rts430xl.lib : div32s.obj (.text)
00019bda 0000003e : asr32.obj (.text:l_asr_const)
00019c18 0000003e : lsr32.obj (.text:l_lsr_const)
00019c56 0000003e sri_frwv_cmd_packet.obj (.text:sri_frwv_cmd_data_recalc_push_delay_ticks)
00019c94 0000003e sri_rtca_data.obj (.text:sri_rtca_static_debug_dump)
00019cd2 0000003e sri_xsums.obj (.text:sri_xsum_8bit_fletcher)
00019d10 0000003c fredi_frwv.obj (.text:fredi_frwv_send_init)
00019d4c 0000003a rts430xl.lib : memcmp.obj (.text:memcmp)
00019d86 00000038 fredi_io.obj (.text:init_GPS_uart)
00019dbe 00000038 fredi_io.obj (.text:init_MILES_uart)
00019df6 00000038 fredi_io.obj (.text:init_diag_uart)
00019e2e 00000038 fredi_io.obj (.text:init_uart)
00019e66 00000038 sri_debug.obj (.text:sri_assert_do)
00019e9e 00000038 sri_m2k_send.obj (.text:sri_m2k_send_init)
00019ed6 00000036 sri_frwv_packet.obj (.text:DoDamageCmd)
00019f0c 00000036 sri_frwv_cmd_packet.obj (.text:sri_frwv_cmd_packet_check_current_tdma_values)
00019f42 00000036 sri_frwv_cmd_packet.obj (.text:sri_frwv_freq_data_init)
00019f78 00000034 rts430xl.lib : _printfi_min.obj (.text:_div)
00019fac 00000034 sri_quart.obj (.text:quart_getrxbytesavail)
00019fe0 00000034 sri_pparse.obj (.text:sri_pparse_packet_peek_idx)
0001a014 00000032 rts430xl.lib : memccpy.obj (.text:memccpy)
0001a046 0000002e : vsnprintf.obj (.text:_outc)
0001a074 0000002e fredi_qhandlers.obj (.text:fredi_qhandlers_UBLOX_i)
0001a0a2 0000002c rts430xl.lib : div16s.obj (.text)
0001a0ce 0000002c sri_frwv_cmd_fill.obj (.text:sri_frwv_cmd_fill_READ_ROM_TDMA)
0001a0fa 0000002c sri_frwv_cmd_fill.obj (.text:sri_frwv_cmd_request)
0001a126 0000002c sri_frwv_packet.obj (.text:sri_frwv_packet_insert_slotcmd)
0001a152 0000002a sri_m2k_display.obj (.text:dynamicFormatter)
0001a17c 0000002a rts430xl.lib : memcpy.obj (.text:memcpy)
0001a1a6 0000002a sri_m2k_display.obj (.text:picSerialNumberFormatter)
0001a1d0 0000002a sri_test_harness.obj (.text:sri_test_harness_func_result)
0001a1fa 0000002a sri_m2k_display.obj (.text:ternSerialNumberFormatter)
0001a224 00000028 rts430xl.lib : sprintf.obj (.text:_outs)
0001a24c 00000028 fredi_frwv_status.obj (.text:fredi_frwv_status_init)
0001a274 00000024 sri_msgqueue.obj (.text:sri_msgqueue_isfull)
0001a298 00000022 fredi_qhandlers.obj (.text:fredi_qhandlers_default_o)
0001a2ba 00000022 rts430xl.lib : mult32_f5hw.obj (.text)
0001a2dc 00000022 sri_frwv_cmd_fill.obj (.text:sri_frwv_cmd_fill_ID)
0001a2fe 00000022 sri_frwv_cmd_fill.obj (.text:sri_frwv_cmd_fill_VERSION)
0001a320 00000022 sri_queue.obj (.text:sri_queue_isfull)
0001a342 00000022 sri_tspi_data.obj (.text:sri_tspi_data_init)
0001a364 00000020 rts430xl.lib : memset.obj (.text:memset)
0001a384 0000001e sri_m2k_msg.obj (.text:sri_m2k_msg_damage_source_by_subcode)
0001a3a2 0000001e sri_msgqueue.obj (.text:sri_msgqueue_getavail)
0001a3c0 0000001e sri_tspi_data.obj (.text:sri_tspi_debug_dump_time)
0001a3de 0000001c sri_frwv_cmd_fill.obj (.text:sri_frwv_cmd_request_init)
0001a3fa 0000001c sri_frwv_cmd_fill.obj (.text:sri_frwv_cmd_request_set_RAM_frametable)
0001a416 0000001c sri_msgqueue.obj (.text:sri_msgqueue_isempty)
0001a432 0000001c sri_queue.obj (.text:sri_queue_isempty)
0001a44e 0000001a rts430xl.lib : strlen.obj (.text:strlen)
0001a468 00000018 sri_frwv_cmd_packet.obj (.text:sri_frwv_cmd_data_recalc_numUsedFrames)
0001a480 00000018 sri_frwv_dual_parse.obj (.text:sri_frwv_dual_parse_reinit_state_machine)
0001a498 00000018 sri_xsums.obj (.text:sri_xsum_16bit_sum)
0001a4b0 00000018 sri_xsums.obj (.text:sri_xsum_8bit_blockparity)
0001a4c8 00000016 rts430xl.lib : div16u.obj (.text)
0001a4de 00000016 : mult16_f5hw.obj (.text)
0001a4f4 00000016 sri_msgqueue.obj (.text:sri_msgqueue_getlength)
0001a50a 00000016 sri_queue.obj (.text:sri_queue_getlength)
0001a520 00000014 rts430xl.lib : sprintf.obj (.text:_outc)
0001a534 00000014 sri_xsums.obj (.text:sri_xsum_null)
0001a548 00000012 sri_imiles_send.obj (.text:show_send_buf)
0001a55a 00000010 sri_m2k_display.obj (.text:sri_m2k_display_get_rit_init)
0001a56a 00000010 sri_m2k_display.obj (.text:sri_m2k_display_set_rit_receive)
0001a57a 00000010 sri_m2k_display.obj (.text:sri_m2k_setVestType)
0001a58a 00000010 sri_m2k_display.obj (.text:sri_m2k_set_m2k_event_disable_state)
0001a59a 0000000e fredi_qhandlers.obj (.text:fredi_qhandlers_init)
0001a5a8 0000000a sri_time.obj (.text:time_go)
0001a5b2 00000008 fredi_qhandlers.obj (.text:fredi_qhandlers_handle)
0001a5ba 00000008 sri_frwv_cmd_packet.obj (.text:sri_frwv_cmd_packet_numUsedFrames)
0001a5c2 00000008 sri_frwv_cmd_packet.obj (.text:sri_frwv_cmd_packet_push_delay_ticks)
0001a5ca 00000008 sri_frwv_packet.obj (.text:sri_frwv_ediSerial)
0001a5d2 00000008 sri_m2k_display.obj (.text:sri_m2k_display_get_rit_receive)
0001a5da 00000008 sri_test_harness.obj (.text:sri_test_harness_is_in_test)
0001a5e2 00000006 sri_frwv_dual_parse.obj (.text:sri_frwv_dual_parse_client_done)
0001a5e8 00000006 sri_imiles_send.obj (.text:sri_imls_get_xmit_queue)
0001a5ee 00000006 sri_m2k_send.obj (.text:sri_m2k_get_xmit_queue)
0001a5f4 00000004 rts430xl.lib : pre_init.obj (.text:_system_pre_init)
0001a5f8 00000004 : exit.obj (.text:abort)
0001a5fc 00000002 : _lock.obj (.text:_nop)