One input to MSP430F2001 comparator a+ is 1.25V reference and other input is a voltage divider off a DC source we are wanting to determine when it exceeds a certain value. When the divided DC source input is below reference, it works fine but when it tries to go above the reference voltage, it's clamped at reference voltage level. Need it to be able to go above the reference voltage also. Supply to part is 3.6Vdc.