This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi,
There are 2 questions about SYSCONFIG.
About 'udpecho_MSP_EXP432E401Y_tirtos_ccs_syscfg'.
ti/simplelink_msp432e4_sdk_2_20_00_20/examples/syscfg_preview/rtos/MSP_EXP432E401Y/ns/udpecho/tirtos/ccs
Q1.
I'd like to set the GPIO Output as 108pin for LED.
But, 108pin aren't shown to GPIO Pin menu.
Q2.
I'd like to set the Link OK LED of EMAC as 43pin.
I'd like to set the TX/RX Activity LED of EMAC as 46pin.
But, these pins aren't shown to menu.
61pin and 63pin are used by EPI, so I'd like to change it.
Thank you.
I am still working with the larger team to understand the sysconfig architecture. You can create custom board definitions in the .meta directory found in the SDK.
C:\ti\simplelink_msp432e4_sdk_2_30_00_14\source\ti\boards\.meta
The new board must then be referenced in the CCS project.
I will provide an update on 10/27 with more details on the file edit process.
Regards,
Chris
**Attention** This is a public forum