Other Parts Discussed in Thread: MSP430F5438, MSP430F5419
Hello,
My simple question is, what is the initial setting of the MSP430F5438 or MSP430F5419 in regard to the clock and to the program that it runs when it comes from the factory?
My guess on clock is that it uses the internal ~ 32 kHz oscillator. But if there is a crystal tied to XT1 and XT2, does it then try to use it?
My guess on program is that it simply goes into some low power mode and sleeps. Of course, I will program the devices, but I typically program in place and I would like to know what it is running the first time that I apply power, when it's on my circuit board.
I also assume that all peripherals are off, and that all pins are set as inputs in digital mode. Is this correct? More specifically, for example, are the pins that have the ADC input function really acting as digital I/O inputs, and therefore they could draw some current if they are connected to an intermediate voltage? On my board, for example, I have a 2.048V reference connected to the Vref+ pin. Before I first program the chip, will this cause a problem, and how much current could it possible draw?
I have not found the information about either of these in the data sheets. Can someone please point this out to me as well?
Thank you for any help on my several questions, expert friends.
Sage