Part Number: MSP430F6659
Hi,
I am working with a unit that have th MSP430.
I got with the unit an INVOKE file to open before opening the SW of the MSP (to burn the code).
As I understand (and i do not understand much...) in order to burn the code to the MSP , teh INVOKE file take the MSP in the device manager from the PORT list (PID=0300) to the HID list (PID=0200).
My problem is that after I click on the invoke file - I still see the MSP in the PORT list in the device manager, and I must unplug the USB from the PC and plug it again, in order to see the device under the HID list , to be able to burn the code.
Are you familiar with such a case ? do you have any suggestion why it is happen and how to solve it ?
Regards,
Shalom Cohen