Hello,
I intend to use this uC as a device that will be powered on once connected to the host and intend to use full-speed, not high-speed. I currently have a common mode choke, ESD protection diodes, and a 100ohm resistor on the VBUS line to limit ESD damage. Looking through the uC documentation I don't think I saw any information relating to pull-up/pull-down resistors on the USB0DM and USB0DP lines, but I've read sources that say otherwise. Do I need them?
Below is a snippet of the portion of the schematic. Thank you and I apologize if this information is in the documentation somewhere and I have missed it.