This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2418: When Flasher writes the TI-txt file to the device, an error 60 is displayed and it fails.

Part Number: MSP430F2418


Dear Britta,


Thank you for your help in solving this problem.
I looked at other similar reports that have been posted.
The problem seems to be inside MSP430.dll, but seems to be being addressed by MSPFlasher version 1.3.14.
I am using MSPFlasher version 1.3.15.
Therefore, I think MSP430.dll is using the version that is being handled.

There was progress.
I turned on and off the device (MSP430F2418) side and reconnected the MSP - FET Flash Emulation Tool.
After that, I succeeded when writing the TI-txt file again with Flasher.
When writing fails, the TI-txt file and Flasher version are the same.
Possible causes were connection failure of the MSP - FET Flash Emulation Tool or was the device side movement unstable?
Please tell me if you have any information.
Thanking you in advance.

Thu Oct 18 13:57:53 2018: * -----/|-------------------------------------------------------------------- *
Thu Oct 18 13:57:53 2018: *     / |__                                                                   *
Thu Oct 18 13:57:53 2018: *    /_   /   MSP Flasher v1.3.15                                             *
Thu Oct 18 13:57:53 2018: *      | /                                                                    *
Thu Oct 18 13:57:53 2018: * -----|/-------------------------------------------------------------------- *
Thu Oct 18 13:57:53 2018: *
Thu Oct 18 13:57:53 2018: * Evaluating triggers...done
Thu Oct 18 13:57:53 2018: * Checking for available FET debuggers:
Thu Oct 18 13:57:53 2018: * Found USB FET @ COM9 <- Selected
Thu Oct 18 13:57:53 2018: * Initializing interface @ COM9...done
Thu Oct 18 13:57:54 2018: * Checking firmware compatibility:
Thu Oct 18 13:57:54 2018: * FET firmware is up to date.
Thu Oct 18 13:57:54 2018: * Reading FW version...done
Thu Oct 18 13:57:54 2018: * Setting VCC to 3000 mV...done
Thu Oct 18 13:57:59 2018: * Accessing device...done
Thu Oct 18 13:57:59 2018: * Reading device information...done
Thu Oct 18 13:57:59 2018: * Loading file into device...done
Thu Oct 18 13:58:00 2018: * Verifying memory (C:\FIRMWARE\Bin\Program_V07.txt)...done
Thu Oct 18 13:58:01 2018: *
Thu Oct 18 13:58:01 2018: * ----------------------------------------------------------------------------
Thu Oct 18 13:58:01 2018: * Arguments   : -w C:\FIRMWARE\Bin\Program_V07.txt -v -e ERASE_MAIN
Thu Oct 18 13:58:01 2018: * ----------------------------------------------------------------------------
Thu Oct 18 13:58:01 2018: * Driver      : loaded
Thu Oct 18 13:58:01 2018: * Dll Version : 31001000
Thu Oct 18 13:58:01 2018: * FwVersion   : 31000003
Thu Oct 18 13:58:01 2018: * Interface   : TIUSB
Thu Oct 18 13:58:01 2018: * HwVersion   : U 3.0
Thu Oct 18 13:58:01 2018: * JTAG Mode   : AUTO
Thu Oct 18 13:58:01 2018: * Device      : MSP430F2418
Thu Oct 18 13:58:01 2018: * EEM         : Level 3, ClockCntrl 2
Thu Oct 18 13:58:01 2018: * Erase Mode  : ERASE_MAIN
Thu Oct 18 13:58:01 2018: * Prog.File   : C:\FIRMWARE\Bin\Program_V07.txt
Thu Oct 18 13:58:01 2018: * Verified    : TRUE
Thu Oct 18 13:58:01 2018: * BSL Unlock  : FALSE
Thu Oct 18 13:58:01 2018: * InfoA Access: FALSE
Thu Oct 18 13:58:01 2018: * VCC OFF
Thu Oct 18 13:58:01 2018: * ----------------------------------------------------------------------------
Thu Oct 18 13:58:01 2018: * Powering down...done
Thu Oct 18 13:58:01 2018: * Disconnecting from device...done
Thu Oct 18 13:58:01 2018: *
Thu Oct 18 13:58:01 2018: * ----------------------------------------------------------------------------
Thu Oct 18 13:58:01 2018: * Driver      : closed (No error)
Thu Oct 18 13:58:01 2018: * ----------------------------------------------------------------------------
Thu Oct 18 13:58:01 2018: */

**Attention** This is a public forum