Hey guys; haven't found much info here when searching 485. I just want someone to verify my setup. I will be using a Max483 RS485 tranceiver(http://datasheet.octopart.com/MAX485ESA-Maxim-datasheet-51242.pdf) for communications with my MSP430(msp430f2619).
I have pin 3.4(USCI A0 transmit output going into pin 4(DI) of the Max483, pin 3.5(USCI A0 receive data input) going to pin 1(RO) of the tranceiver. For the driver/receiver enables I have it going to 2 general i/o pins. Is this configuration ok?
Also if anyone can point me to some info i may not be seeing on msp430/rs485 interfacing that would be awesome.
Thanks,