Part Number: MSP430F2274
Other Parts Discussed in Thread: SIMPLICITI
Tool/software: Code Composer Studio
Hello
I am trying to build simpliciti examples for ez430-rf2500 on WIN10 with CCS v7
On the folder with the simpliciti files( C:\ti\ccsv7\tools\compiler\ti-cgt-msp430_16.9.6.LTS\lib ) there are 3 libraries:
1) Which library should i use?
rts430_eabi.lib
rts430x_lc_sd_eabi.lib
rts430x_lc_rd_eabi.lib
2) what is the difference between them?
I am able to build using rts430_eabi.lib but the example program simple peer to peer does not run properly
The code is stuck in SMPL_Init(sRxCallback) inside the function: *nwk_buildFrame(uint8_t port, uint8_t *msg, uint8_t len, uint8_t hops)
at a line: while (!(++sTRACTID)) ; /* transaction ID can't be 0 */
What I am doing wrong?
Does someone have any experience with that?
Thank you
Maoz Loants