Part Number: MSP430F5324
Other Parts Discussed in Thread: MSP430F5326, MSP430F5328
I have qualified the MSP430F5324 (6k RAM, 64k Flash) device in my design. I would like to add the larger MSP430F5326 (8k RAM, 96k Flash) and MSP430F5328 (10k RAM, 128k Flash) as alternate parts to use in my production build in case of part unavailability, but I want to know that there are absolutely no other differences in the devices than the RAM and Flash size differences. The errata lists for the 3 part numbers are identical for all silicon revisions, so I suspect that they are in face identical silicon. Is this in fact the case? I have used other TI devices that were labeled differently, but were in fact the same part, only the more expensive part had additional features qualified and tested.