Part Number: MSP430F248
Hello Sir,
We used TI MCU MSP430F248 and found some issue of this chip initializaiton.
1) The board we designed used 3.6864MHz oscillator, so of course we set register BCSCTL3 : Bits 7-6(XT2 range select) : 10 3-to 16-MHz crystal or resonator
2) MSP430F248 head file in IAR , its comments seems has some conflict with User Manual ( But I think this definition in User Manual should be right )
3) Anyway, my question is : when we selected "XT2S_2" configuration after power on and run the whole system , its power consumption = 2.6mA
when we not set this Bits7-6 (default setting after power on should be 00 ), its power consumption = 1.6mA
when we selected "01" (1- to 3-MHz crystal or resonator ), its power consumption about 1.6mA .
But the actual external crystal = 3.6864MHz , so would you mind help us to analyze why cause this abnormal issue?
Hope your response ASAP.
Thanks.
Best Regards,
Vincent