Hi all,
With the configuration shown below, VDD_3.0 V and VDD_1.8 V are always on and the A-side and B-side are set to HiZ by setting OE of TXS0108 Low.
How do I set the I/O of the MSP430 to achieve lower power consumption including leak current from I/Os?
If the MSP430 I/O remains INPUT mode, the input becomes indeterminate. Should I switch to OUTPUT mode?
If OUTPUT mode is selected, output is Low or High?
Regards,
Toshi