This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430FR2311: Duty cycle for PWM above 350kHz

Part Number: MSP430FR2311

Tool/software: Code Composer Studio

i cant get perfect duty cycle for waveform above 350 KHZ frequency

when i changed from 10%-90% the duty cycle produced will be 33% and 66% 

**Attention** This is a public forum