Part Number: MSP430F5528
Tool/software: Code Composer Studio
Hi, I am using tdc1000-tdc7200evm to communicate with other board through uart from GPIO3\GPIO4. I can read from the oscilloscope that there is data transmitted, and I connect RX TX with a wire. However, the program cannot jump into RX interrupt. I found the interrupt enable register was 0 but I enabled interruptions in my code.
By the way, I have enabled system interruptions.
Here are my codes and the value of UART registers:
void InitUART(void){
UCAxCTL1 |= UCSWRST; // **Stops USCI state machine**
UART_PxREN &= ~(UART_TX_PAD|UART_RX_PAD); //Disable port pull resistors
UART_PxDIR &= ~UART_RX_PAD; // Configure P4.5 as input
UART_PxDIR |= UART_TX_PAD; // Configure P4.4 as output
UART_PxSEL |= (UART_TX_PAD|UART_RX_PAD); // Px.x & Px.X = USCI_Ax TXD & RXD
UCAxCTL0 = 0x00; // No parity, 8-N-1 mode
UCAxCTL1 |= UCSSEL__ACLK; // Select 12MHz ACLK as clock source for the UART
UCAxBR = UART_BAUDRATE_REG; // defines baudrate
UCAxMCTL = (UCBRF_0|UCBRS_1); // Modulation UCBRSx = 1 //vishy: 115200 baudrate selection @ 12MHz
// UCAxMCTL = (UCBRF_0|UCBRS_0); // Modulation UCBRSx = 1 //vishy: 230400 baudrate selection @ 12MHz
UCAxIFG &= ~UCAxRXIFG; //Clear RX IFG (Interrupt flag register)
UCAxIFG &= ~UCAxTXIFG; //Clear TX IFG (Interrupt flag register)
UCAxIE |= UCAxRXIE +UCAxTXIE; // Enable USCI_A1 RX interrupt
UCAxCTL1 &= ~UCSWRST; // **Initialize USCI state machine**
}
#pragma vector=UCAxRX_VECTOR;
__interrupt void receiveUART(void)
{
unsigned short i;
unsigned char TimeOutCounter = 0;
if (UCAxRXIFG)// USCI_A0 RX buffer ready?
{
open_flag=UCAxRXBUF;
} //wait until Tx buffer is empty
UartRx_flag = 1;
}
What can I do?