Part Number: MSP430F5438A
Hello,
I am trying to collect data from the following optical dust sensor:

According to page 5 of the datasheet, I generated the correct PWM signal using timer A for input PIN 3 of the sensor and observed the signal in my oscilloscope. Now at the same page Figure 2, they talked about the output pulse sample timing. Anyone can help me understand how should I set up my ADC12 for this? Few queries regarding this:
1. Should my sample and hold time be 0.28ms?
2. If so then should I wait for next 0.04ms + 9.68ms to collect my next ADC value as the input pulse needs that much time to arrive?
3. If 1 and 2 are correct, how can I set up my ADC for this?
Thanks,
Row