This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Temperature, Humidity and Communication MCU

Hi All,

I hope everything is going well.

I have a very simple application--basically I need 3 temperature and 2 humidity inputs, and need to control 2 relays based on the input values (Need 9 such systems). Also, I need to communicate the temperature and humidity data, as well as the status of the relays (on/off) to a Master controller, from where that data should be readable via a Dashboard or some sort of GUI.

Which MCUs will be suitable for this project? Which communication protocol should be used? Simply the CAN protocol? Or Modbus TCP? Or some other?

I have never actually worked on a professional level with a MCU, so really need some advice.


The block diagram may help as well..

**Attention** This is a public forum