This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/MSP430FR2522: MSP430FR2522IPW16 online simulation, hang up in MAP_CAPT_powerOn () function.

Part Number: MSP430FR2522

Tool/software: TI C/C++ Compiler

I use the CapTIvateDesignCenter program, CPU uses msp430fr2522.The compiler I use is iar7.1.Now the problem is to download the generated program code directly to my target board without any change. It appears that the program can not be executed down after single step execution to MAP_CAPT_powerOn(). The error prompt is communication error. I use the program downloaded by SBW mode. If this function is commented out, no error is prompted when other statements are executed. What is the situation?

**Attention** This is a public forum