This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6989: LCD character #5 not working

Part Number: MSP430FR6989

Hello, 

I was given a board by a TI employee to work with and upon running the startup demo I noticed that the 5th character has three segments not working. When I attempt to have it output an "8" I get a reverse "C" instead. This means the left vertical segments as well as the middle horizontal segment are not working. Is there anything that could cause this besides a LCD failure, broken resistor or other intermediary IC that could be changed. 

Thanks

Kas

**Attention** This is a public forum