Tool/software: Code Composer Studio
Hi,
I'm trying to hook up an External XDS110 with MSP-EXP432P401R. But the green LED102 stops glowing as soon as I connect the 10 pin debug probe from the XDS110 to the MSP432.
This is the procedure I have followed:
1.Remove TDI,TDO,TMS,TCK,RST Jumpers from J101 Isolation Block
2.Connect the MSP432 to the PC using USB Cable(Green LED Glows)
3.Connect the external XDS110 to the PC using USB Cable
4.Connect the 10 pin debug probe from XDS to MSP432 In port. The Green LED stops glowing and the on board debugger starts getting heated up.
Note: The board works fine when using the on board debugger. The issue is seen only when I try to connect an external XDS110
Thanks,
Aishwarya