This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Sir
Use MSP-FET. The chip MSP430FR2110 cannot be find Spy-Bi-Wire (2-wire JTAG) debug protocols.Use IAR7.12 and MSP430 flasher.
Hello Lei,
if you would like to share some non-public information with us, there is a way to do so in the forum. Please send me a friendship request. Then you can send me private messages with non-public content.
Upfront some additional indications on what could help us resolving the issue:
- supply of the device to be programmed
- schematics of the setup, if not used with the original target board from TI
- length of cable connections (probably visible from the pictures you intend to provide
- is it just one unit, which is failing to connect, or have you tried multiple with the same result?
Many thanks in advance.
Best regards
Peter
Hi Lei,
In addition to Peter's questions above, can you confirm that your connections look as the picture below?
Do you have any differences in any of the connections or components?
It seems like they are using their own board, but do you or the customer have any target board or Launchpad? If so, have you tried connecting the MSP-FET to those boards?
Have you used the MSP-FET with any other boards/devices to make sure it works?
Regards,
Luis R
**Attention** This is a public forum