This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: cad file

Part Number: MSP432P401R


Hello TI Experts,

Can you help to provide the  CAD file of MSP432P401R?Thank you very much~

I have downloaded the Ultra Librarian software but have problem  opening the file with Altium Designer~

  • Hello,
    There are three packages for this device. LQFP, NFBGA, and VQFN. Which device are you trying to open via the Ultra Librarian?

    Update:  I ran the LQFP package and was able to build the PCB and Sch files.  The readme.txt file generated from Ultra Librarian provides a link to a youtube video which you might find helpful.

    1. After running the Ultra Librarian export for the first time,
    you will need to copy the following files into an area where
    they can be accessed for all future translations. They are script
    files that Altium will need to be able to find.
    a. UL_Form.dfm
    b. UL_Form.pas
    c. UL_Import.pas
    d. UL_Import.prjScr

    2. The above script file will need to be run from within Altium.
    This can be done by going to File, Open and selecting the
    UL_Import.PrjScr file stored above.

    3. Select the UL_Form.pas file form the new project that has loaded,
    and then select runfrom the drop down menu. You will need to select
    the form again. Run the form.

    3. When the script is run, it will ask you for the file name of the
    Ultra Librarian file to run. You should select the latest file
    produced with a date code (for instance 2010-02-17_23-12-34.txt).

    4. The script will open a new Integraged Library project and import
    the Ultra Librarian data into it. When complete a message box
    will pop up saying that import is done.

    For additional information, please visit this site:
    http://www.accelerated-designs.com/help/Altium_import.html

    For a video tutorial, please visit:
    http://youtu.be/pih50yx9HYU


    Regards,
    Chris

  • Hi thank you very much for your kindly help~~
    I am using this part MSP432P401RIPZR,maybe something is wrong with my computer~
  • lqfp.zip

    Please find the attached.  

    Regards,

    Chris

**Attention** This is a public forum