This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2553: Code for built-in program on MSP430G2ET LaunchPad?

Part Number: MSP430G2553

Hi there,

Where can I find the code for the program already Flashed into the device on the MSP430G2ET LaunchPad?

I removed the device and plugged it into a breadboard, along with power, ground and an LED+resistor on Pin 1.0, but it didn't flash like it did on the LaunchPad, so I'm wondering if there's another dependency.

Thanks!

Jason

**Attention** This is a public forum