Tool/software: Code Composer Studio
I want to connect TXD and RXD pins of MSP432 to Bluetooth HC05. The thing is I cannot locate port pin P1.2 and P1.3 on the board. Is there any way to tapout those two pins from MSP432 or do I need to use another EUSCI module which has its port pins exposed? So, another question being if I use P3.2 and P3.3 belonging to EUSCI_A2. are they internally connected to USB to UART bridge ?