Part Number: MSP432P401R
Hello, I'm new to programming the MSP432 and I have problems with my code. What I want to achieve is getting audio from my microphone electret (Adafruit MAX9814), sample the signal at 44.1 kHz (the signal would be converted from analog coming from the microphone to digital), convert that digital signal back to analog and output it to a speaker so I can listen to the sound. I'm not hearing anything but static so far. Can I get guidance? I'll leave my code below.
#include "msp.h" #include <stdint.h> void main(void) { WDT_A->CTL = WDT_A_CTL_PW | WDT_A_CTL_HOLD; // stop watchdog timer //GPIO Setup P4->DIR &= ~(BIT7);// Analog input channel A6 P4->SEL0 |= BIT7; // Enable A/D channel A6 P4->SEL1 |= BIT7; // P4.7 - analog input P5->DIR |= BIT4; // Output to speaker P5->SEL0 |= BIT4; //while(PCM->CTL1 & PCM_CTL1_PMR_BUSY); //PCM->CTL0 = PCM_CTL0_KEY_VAL | PCM_CTL0_AMR__AM_LDO_VCORE1; //while(PCM->CTL1 & PCM_CTL1_PMR_BUSY); //Set clock to 24 MHz using DCO CS->KEY = CS_KEY_VAL; //Unlock CS registers CS->CTL0 = CS_CTL0_DCOEN | CS_CTL0_DCORSEL_4; //Choose 24 MHz clock speed CS->CTL1 = CS_CTL1_SELS_3 | CS_CTL1_SELM_3 ; //Use DCOCLK as source for MCLK, SMCLK + HSMCLK CS->KEY = 0; //Re-lock CS registers // ADC14 Setup ADC14->CTL0 &= ~ADC14_CTL0_ENC; // Reset ENC bit for configuration ADC14->CTL0 = ADC14_CTL0_PDIV_1 | // Pre-divide clock by 4 ADC14_CTL0_SHS_1 | // Timer A0 trigger ADC14_CTL0_SHP | // Pulse mode ADC14_CTL0_DIV_5 | // divide clock by 6 ADC14_CTL0_SSEL_3 | // ADC clock source is MCLK ADC14_CTL0_CONSEQ_2 | // Repeat-single channel ADC14_CTL0_SHT0_2 | // Sampling length of 16 ADC clock cycles ADC14_CTL0_ON; // ADC module on ADC14->CTL1 = ADC14_CTL1_RES_3; // 14-bit resolution ADC14->MCTL[0] = ADC14_MCTLN_INCH_6; // ref+ = AVcc, channel = A1 // Timer_A0 Setup TIMER_A0->CCTL[0] = TIMER_A_CCTLN_CCIE; //Enable CC interrupt TIMER_A0->CTL = TIMER_A_CTL_TASSEL_2 | // SMCLK as source for timer TIMER_A_CTL_ID_1 | // Divide clock by 2 -> 48 MHz / 2 = 24 MHz TIMER_A_CTL_MC_1 | // Up mode TIMER_A_CTL_CLR | // Clear timer count TIMER_A_CTL_IE; // Enable overflow interrupt TIMER_A0->CCR[0] = 544; // 24 MHz / 44.1 kHz = 544 // T = (TAxCCR0+1) / f_clk = (544+1) / 24 MHz = 2.27x10^(-5) TIMER_A0->CCTL[1] = TIMER_A_CCTLN_OUTMOD_7; // Set/Reset for trigger halfway through the cycle // Enable global interrupt __enable_irq(); NVIC->ISER[0] = 1 << ((ADC14_IRQn) & 31); // Enable ADC interrupt in NVIC module // Wake up on exit from ISR SCB->SCR &= ~SCB_SCR_SLEEPONEXIT_Msk; // Ensures SLEEPONEXIT takes effect immediately __DSB(); while(1) { ADC14->CTL0 |= ADC14_CTL0_ENC | ADC14_CTL0_SC; // Start conversion-software trigger __sleep(); __no_operation(); // For debugger } } void ADC14_IRQHandler(void) { while((ADC14->IFGR0 & ADC14_IFGR0_IFG6) == 0); // waiting for conversion to be done //audio = ADC14->MEM[0]; // Conversion stored in audio variable. P5->DIR ^= BIT4; } //void TA0_A0_IRQHandler(void) //{ // TIMER_A0->CCTL[0] &= ~TIMER_A_CCTLN_CCIFG; //}