Part Number: MSP430FR59721
Other Parts Discussed in Thread: MSP430F249, , MSP430FR5739, SN74LVC1G125
I have setup the registers and believe that they are correct. I have a baud rate of 115200. I am sending a small message with 5 bytes. I can observe the transmitted data on a CRO and it is correct. I can also connect to a PC and observe it is OK. When I transmit from the PC (using Tera term) I do not receive the interrupt. I can see the waveform on the CRO at pin 1 on the MCU. I have GIE set and the receive interrupt enabled. I have no parity set.
Any suggestions would be appreciated.
Thanks
Peter