Other Parts Discussed in Thread: CC2642R
Hi,
Can you recommend microcontroller with below features?
| Power | 1.65V-3.3V |
| Microcontroller Core | 32 Bit |
| Dhystone MIPS | 1.65 DMIPS/MHz |
| Program Memory | 512 KB Flash |
| RAM | 64/96 KB SRAM |
| FSMC (Flexible Static Memory Controller) for NAND Flash Interface |
Only SDRAM interfacing pins |
| USB | Host/Function/OTG |
| Maximum Frequency | 100 MHz |
| UART | 4 |
| SPI | 3 |
| I2C | 3 |
| ADC | 12/16 BIT |
| BLE | YES |
| WatchDog | YES |
| OTG | YES |
Thanks,
Murugavel.S