Tool/software: TI C/C++ Compiler
I have some questions about the compilation of structs.
the main problem is that i want yo make a method to copy a value to a struct through a pointer and it can't be done.
the function have three arguments like this.
int ReadRegister (unsigned char *Buff, int start_register, unsigned int count)
i want to put the read value to a struct wich is pointed by Buff. may i can clarify my doubts with a fragment of code:
typedef struct
{
unsigned char Family_Id;
}InfoId_t;
int ReadRegister (unsigned char *Buff, int start_register, unsigned int count)
/*----------------------------------------------------------------------------*/
/** \brief
Reads a register from the device as many bytes as you would like.
*******************************************************************************/
{
BuffT[0] = start_register & 0xff; //LSB
BuffT[1] = (start_register >> 8) & 0xff; //MSB
Write(TACTI2C_SLVADDR, BuffT, 2); // This write register you want to read
Read(SLAVEADDRESS, RxBuff, count)
for(int i=0; i<count; i++)
{
*Buff = RxBuff[i];
Buff++;
}
return OK;
}
void main() { InfoId_t info; unsigned char *ucRxBuff; ucRxBuff = &info.Family_Id error = ReadRegister (ucRxBuff, 0x00, sizeof(InfoId_t)); return 0; }
the problem in here is that the values are read correctly but when i put the value passing through by pointer info.Family_Id has no value associated.
anyone knows how is this posible? i mean, i suspect that the compiler have some part of fault but but i am not sure. The values are read correctly because i can see making debug all the values in an array
putted inside the fucntion read(), but when i go out the method the value are not copied to info.Family_Id.
Regards