Part Number: MSP430F6736A
Sir, we are working as E-meter project. MSP430F6736A, this TI ic is suited for my application.
your datasheet is mentioned, When CT or shunts are used, make sure the voltages across CUR2+ and CUR2- does not exceed 920 mV
my doubt is,
1.if possible to connect EVM device for my Machine (5A) for testing purpose and also know the maximum Amps (load) rating?
2.If possible to interface my own Current sensor(100 Amps) in EVM? possible means, how to interface?
Please send soon...