Other Parts Discussed in Thread: TRF7970A, RF430FRL152HEVM, RF430FRL152H, LMT70, TIDA-00721
Hello,
I am making a prototype of the TIDM-RF430FRLSENSE using the same components but trying out a different analogue sensor. I intend to use CCS and use the JTAG interface for programming the chip using the MSP-FET430UIF programmer. I am also thinking of using the TRF7970A+MSP-EXP430G2 as the reader. I had a look at the firmware's guide and a few example initialization codes (Default / NFC Only), and I was wondering whether I could just use the NFC project code and insert the code for the sensor into the main function to make the device work? I read that the main function already exists in the ROM, so I am also not sure if I have to repeat that in the code I'll use or not. If yes, where can I get that?