Part Number: MSP430FR2311
Hi,
What's the resolution of eCOMP? My customer want to compare two external input signal at 100mV difference. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR2311
Hi,
What's the resolution of eCOMP? My customer want to compare two external input signal at 100mV difference. Thanks.
Hi Daniel
That can be work with 100mV difference.
You can just calculate the resolution of the eCOMP like this: Resolution=Voffset +Vhys ; Voffset means Input offset voltage, Vhys DC input hysteresis
the values you can refer to the msp430fr2311's datasheet
So the minimum can be 30 mV but the robustness is worse without the hysteresis.
Best regards
Gary
**Attention** This is a public forum