This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP-GANG430
Hi,
I am using Gang Pro ARM where i upload my firmware file using 'F_AutoProgram()' function from 'GANGPROARM_API' class. Once I upload firmware file I can see file data inside flash block of gang software.
I want to get data from the specific address and change data data. But i am not getting any specific function to do that for C# in 'GANGPROARM_API' class. Can you please suggest any way to get data from flash block
Thanks & regards,
Shraddha K
Hi Shraddha,
The GangPro-ARM programmer is not the TI MSP-GANG Programmer. Please send me your email address then we can reply for it - support@elprotronic.com
Best regards,
Gregory Czajkowski
Elprotronic Inc.
gregory@elprotronic.com
Hello,
In my project I am currently working on two different hardware devices, MSP-GANG430 and GANG PRO-ARM.
----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
MSP Gang430:
----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
In my first module i was using MSP-GANG430 device. In that module, my requirement was to load firmware file on the GANG Programmer. To accesss 'MSP GANG430' device I used "GANG430.dll" functions with user guide mentioned below:
technodocbox.com/.../71324740-Msp430-gang-programmer-msp-gang430-user-s-guide.html
In the user guide mentioned in the link, there was a function called 'GangLoadImage', which writes data from a file either of type TI-txt or of type Intel-hex(auto-detect) into the MSP-GANG430 programming unit’s image flash memory directly.
MSP-GANG430:
-----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
GANG PRO-ARM
------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Now in my second module i am using GangPro-ARM. And want to implement the same functionality of firmware upload. And after file load i need to change some file data
at a particular address from flash memory. I am using 'GangProARM-FPAsel.dll' to access this Gang software. I am using user guide 'GangPro-ARM API-DLL User's Guide' downloaded from following link :
www.elprotronic.com/productdata
My question is as i mentioned above regarding MSP Gang 430, in Gang Pro ARM, there is no direct function to access flash memory data. What I need to do is :
1. load file using F_ConfigLoad
2.Then i need to copy flash memory data to Gang buffer using 'F_Copy_Flash_to_Gang_Buffer'
3. Then I need to read data from gang buffer using 'F_Get_Byte_from_Gang_Buffer'.
4. Then only I can edit data present in the gang buffer using 'F_Put_Byte_to_Buffer'.
4. After an edit, I again need to copy Gang Buffer data to the Flash memory using 'F_Copy_Buffer_to_Flash'.
I want direct functionality, which can allow me to edit data directly to the flash memory of GANGPro-ARM.
Thanks and Regards,
Shradha K
**Attention** This is a public forum