This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Our customer assume OTA firmware update using CC3220MODA.
Microcontroller is MSP430FR6879.
Now SLAA721B is referred to implement OTA function.
1. Is it correct materials to implement OTA with these devices?
2. This app report says
"FRAM microcontrollers using either universal asynchronous receiver/transmitter (UART) communication or a serial peripheral interface (SPI) bus and CC110x RF transceivers to accomplish over-the-air downloads (OAD)"
Is it possible to update firmware over SPI? (MSP430 and CC3220 is connected with SPI in the application)
BestRegards
**Attention** This is a public forum