Other Parts Discussed in Thread: MSP430FE427
Hi...
i am working on calibration. i tried my board without calibrating and saved values measured by MSP and Monofase Digital Electric meter.
The values are like this:
While Msp reached 0.088 kWh, Reading value on the Meter was 0.075. So i need to calibrate. This point is clear.
Value of single measurement rev 1.0
4: Voltage (V) ':228.755
5: Current (A) /:0.154
6: Peak Voltage (V/:315.946
7: Peak Current (A/:0.222
8: Frequency (Hz) ':50.008
9: CosPhi ':0.997
10: Power (kW) #:0.000000
11: Energy (kWh) ':0.088
We have two anolog inputs on MSP. One of them is Voltage input and other Current input.(V1+, V1-, I1+ , I1-).
The msp knows the voltage diver resistor's values and shunt resistor's value by parameter.h file.
These informations must be enough to correct measurement and calculations.
Why do we have to calibrate the MSP430FE427?
My second questions is:
For example i produce Energy meter card 100 or more piece. They are complately same product of serial pruduction.
Does i have to calibrate one by one evry card?
or Calibrate one of them and save offset etc. values. Then load executable file to the all MSPs.
in fact, these questions i asked are about "what kind of way does i use during serial production?"
Thanks....