Part Number: MSP430FR2311
Tool/software: Code Composer Studio
I think there is an error in driverlib for adc.h The channel mappings don't match up with Table 6-16 in www.ti.com/.../msp430fr2311.pdf
I'm trying to use A1 (P1.1) as analog input and so I'm trying to figure out which to use. I'm assuming if the mapping is incorrect I should use ADC_INPUT_VEREF_P since it maps to ADCINCH_1
//***************************************************************************** // // The following are values that can be passed to the inputSourceSelect // parameter for functions: ADC_configureMemory(). // //***************************************************************************** #define ADC_INPUT_VEREF_N (ADCINCH_0) #define ADC_INPUT_VEREF_P (ADCINCH_1) #define ADC_INPUT_A2 (ADCINCH_2) #define ADC_INPUT_A3 (ADCINCH_3) #define ADC_INPUT_A4 (ADCINCH_4) #define ADC_INPUT_A5 (ADCINCH_5) #define ADC_INPUT_A6 (ADCINCH_6) #define ADC_INPUT_A7 (ADCINCH_7) #define ADC_INPUT_A8 (ADCINCH_8) #define ADC_INPUT_A9 (ADCINCH_9) #define ADC_INPUT_TEMPSENSOR (ADCINCH_12) #define ADC_INPUT_REFVOLTAGE (ADCINCH_13) #define ADC_INPUT_DVSS (ADCINCH_14) #define ADC_INPUT_DVCC (ADCINCH_15) //*****************************************************************************