Hi
I am trying to use the MSP430F5529LP to send AT commands[http://www.elecomes.com/images/upload/File/Dot%20AT%20command.pdf], the receiver is essentially a processor[MTDOT-915-xx]. Now the whole setup works wonderfully when using both the boards are powered by USB. However when I try to power both the boards using 3.3V external power source. It doesn't seem to work. Datasheet of both boards say that 3.3V would do? What can be a potential problem?