This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430I2041: msp430i2041

Part Number: MSP430I2041

Tool/software: Code Composer Studio

Dear all,

I want to send a string via UART, the issue is it only sends the first character, I would really appreciate some help in this regards. The code is attached below:

//Intialisation bit:

    //UART
    P1SEL0 |=   BIT2 | BIT3;                // P1.2/3 eUSCI_A Function
    P1SEL1 &= ~(BIT2 | BIT3);

    UCA0CTL1 |= UCSWRST;                    // Hold eUSCI in reset
    UCA0CTL1 |= UCSSEL_2;                   // SMCLK
    UCA0BR0   = 0xAA;                       // 9600 baud
    UCA0BR1   = 0x06;
    UCA0MCTLW = 0xD600;                     // 16.384MHz/9600 = 1706.6667 (See UG)
    UCA0CTL1 &= ~UCSWRST;                   // Release from reset
    UCA0IE   |= UCRXIE;                     // Enable RX interrupt

    // Setting the DCO to use the internal resistor. DCO will be at 16.384MHz
    CS_setupDCO(CS_INTERNAL_RESISTOR);
    CS_initClockSignal(CS_SMCLK, CS_CLOCK_DIVIDER_1);

// Interrupt routine

void USCI_A0_ISR(void)
{
    switch(__even_in_range(UCA0IV, USCI_UART_UCTXCPTIFG)) {
        case USCI_NONE: break;
        case USCI_UART_UCRXIFG:
            u = 0;
            while (!(UCA0IFG&UCTXIFG)); // USCI_A0 TX buffer ready?
            {
                sprintf(randomstr, "%d", p_results_2);// convert p_result_2 to string
                while (randomstr[u] != '\0')
                {
                    UCA0TXBUF = randomstr[u];
                  
                    u++;
                    //UCA0TXBUF = 0x0a;
                }
                UCA0TXBUF = 0x0a;
               
                UCA0TXBUF = 0x0d;
                u = 0;
            }
            break;
        case USCI_UART_UCTXIFG: break;
        case USCI_UART_UCSTTIFG: break;
        case USCI_UART_UCTXCPTIFG: break;
        default: break;
    }
}

Regards

Neal

**Attention** This is a public forum