This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2553: Flash memory sectionalization

Part Number: MSP430G2553


Hi,

I am using MSP430G2553 for my project. In this project I have to take in the user data which is of 256 bytes and store it in non-volatile memory. Also, there are some commands of 256 bytes which I need to store in non-volatile memory. I can't make use of memory segment B,C and D because of the small size. I have heard that we can sectionalize the flash memory for storing the using data with the use of linker commands. Can anyone help me out in sectionalizing and guiding on how to use these linker commands. Or if there is any example for the same.

Thanks

Nitish

**Attention** This is a public forum