Part Number: MSP430FR6989
I am using I2C interface on the MSP430FR6989 launch pad dev board. The UCB1SDA functionality is available on P3.1, P4.0 and P4.6 AND UCB1SCL functionality is available on P3.2, P4.1 and P4.7.
I am using UCB1SDA = P4.0 and UCB1SCL = P4.1.
Q1. How can I ensure I have correctly configured UCB1 I2C functionality for P4.0 and P4.1.
Currently, I am following below steps along with MSP430FR6989 driverlib I2C driver,
1.
// Set P4.0 and P4.1 as Primary Module Function.
GPIO_setAsPeripheralModuleFunctionInputPin(
GPIO_PORT_P4,
GPIO_PIN0 + GPIO_PIN1,
GPIO_PRIMARY_MODULE_FUNCTION
);
2. Initialize Master ( steps 2-4 during enatialize)
i2cParams.selectClockSource = EUSCI_B_I2C_CLOCKSOURCE_SMCLK;
i2cParams.i2cClk = 2000000; // 2MHz
i2cParams.dataRate = EUSCI_B_I2C_SET_DATA_RATE_100KBPS;
i2cParams.byteCounterThreshold = 0;
i2cParams.autoSTOPGeneration = EUSCI_B_I2C_NO_AUTO_STOP;
EUSCI_B_I2C_initMaster(EUSCI_B1_BASE, &i2cParams);
3. Set slave address ( 7 bit dev address)
EUSCI_B_I2C_setSlaveAddress(EUSCI_B1_BASE, I2C_WRITE_ADDR >> 1);
4. // Enable I2C
EUSCI_B_I2C_enable(EUSCI_B1_BASE);
5. Wrte to I2C ( Enable Tx Interupt and first byte and second sencond byte when Tx interupt occurs)
EUSCI_B_I2C_enableInterrupt(EUSCI_B1_BASE, EUSCI_B_I2C_TRANSMIT_INTERRUPT0);
EUSCI_B_I2C_masterSendMultiByteStart(EUSCI_B1_BASE, txData.txBuffer[0] );
The program is stuck during sending first byte at
In function EUSCI_B_I2C_masterSendMultiByteStart()
and code is
while(!(HWREG16(baseAddress + OFS_UCBxIFG) & UCTXIFG))
{
;
}
Q2. Is above sequence correct? what is the correct sequence of instruction?
Thanks in advance.
Rajaram