This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F2252: GPIO Pin toggle LED

Part Number: MSP430F2252

Tool/software: Code Composer Studio

#include <msp430.h>

volatile unsigned int i; // volatile to prevent optimization

int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer
P2DIR |= 0xFF; // Set all pins in port 2 to output direction

while(1)
{
P2OUT ^= 0xFF; // Toggle all port 2 pins using exclusive-OR

i = 50000; // Delay
do (i--);
while (i != 0);
}
}

This is the code I written to toggle all GPIO pins in port 2, but the result is P2.6 and P2.7 pins are not toggled and all other pins are toggled. the same thing I tried for port 1, port 3 and port 4 pins and it is working fine. Can I get to know why it is not working only for these two particular pins.(In my design P2.7 pin used to enable RS485 data).Kindly help me over here.

**Attention** This is a public forum