Other Parts Discussed in Thread: DAC161S055
Tool/software: Code Composer Studio
As, I am working CCS V_8 version and deveolping code for MSP432P401R. I am facing a strange problem regarding overflow. As I have my project chain (ADC-DSP-DAC) in my complete project, I am working to implement a digital bandpass filter on MSP432 of the order of 46th by using floating point feature of controller. ADC input range is (0-2.5V) and I am expecting output range same for DAC but the problem is that when I increased input value more than 2.38V Then it leads to an overflow issue. By changing offset vale on signal generator, this issue can be tackeld up to some limit but it is not a professional solution. By googling, i read some articles regarding data type conversions and followed the given procedure (i.e. int (float+0.5)) but it is not helping me. As, my question is more about c programming but I think It has relation with CCS also.
Overflow is occuring due to last values of output when some values are becoming less than zero.Can you please help me to eliminate this overflow issue ??
Note: I have attached the pictures of output with overflow and without overflow alongside the specific part of code too. Every possible suggestion is highly appreciated.

This two picture are taking at the input of step response to the filter.
AdcInputVoltage = AdcValueDigits*2.5f/16384.0f;
filteredf_output = SincFilter(AdcInputVoltage);
/* if (filteredf_output<0){ DacValueDigits = (uint16_t)(( filteredf_output* 65536.0f/4.096f)+0.5);
}
else {DacValueDigits= (uint16_t)(( filteredf_output* 65536.0f/4.096f));
} */
DacValueDigits = (uint16_t)(( filteredf_output* 65536.0f/4.096f)+.5);
//DacValueDigits = ((uint16_t)(( filteredf_output* 65536.0f/4.096f)+32678.5))-32677;
Regards,
Hasan Nawaz