This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
i have some questions about the ROM Bootloader of MSP432E401Y
1. if the FLASH is empty without any code inside, when power on boot, it will automatically jump to execute the ROM bootloader without any need of HW trigger, is it correct?
2. and how to modify the MAC address if using the ROM bootloader to do the FW upgrade?
3. how to erase the FLASH clean enough so that can let MSP432E4 jump to ROM Bootloader automatically once power on due the the FLASH is totally empty?
Hello Erik,
erik lee2 said:1. if the FLASH is empty without any code inside, when power on boot, it will automatically jump to execute the ROM bootloader without any need of HW trigger, is it correct?
Yes!
erik lee2 said:2. and how to modify the MAC address if using the ROM bootloader to do the FW upgrade?
The ROM Bootloader looks for the MAC address in Flash User Registers. These registers can be modified by using "Uniflash" as shown in the following screenshot.
erik lee2 said:3. how to erase the FLASH clean enough so that can let MSP432E4 jump to ROM Bootloader automatically once power on due the the FLASH is totally empty?
Please refer this forum post on how to erase Flash.
Thanks,
Sai
**Attention** This is a public forum