This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2152: PW and RSA package correlation

Part Number: MSP430G2152

I have just completed a prototype design using the MSP430G2152 in the PW package (TSSOP-14).  The application is generating two PWM signals using TimerA0 on TA0.1 and TA0.2.  On the PW package I chose to route these signals to pins #4 and #6 respectively.  I'm just starting the artwork for the PCB layout but I would like to change the package to the RSA (QFN-16).  Looking at the device datasheet (SLAS722G.pdf), page 3, I noticed that the RSA package is not listing TA0.2 as an available multiplexing option for pin #5.  I'm hoping this is just a 'typo' or was intentionally omitted due to lack of printable space on this page?

Note, page 41 illustrates the P1.4 schematic pin.  TA0.2 is listed as an available option and I don't see any footnotes regarding possible package differences.  So I'm suspecting this option is available.

Thanks for the help.

Bill

**Attention** This is a public forum