Other Parts Discussed in Thread: MSP430FR5964
Hi,
There is an issue about MSP430fr5964 below:
1.When I powered off the power completely, I found it has 0.8V voltage. I check circuit to find when I removed ADC circuit, the circuit worked nomally.The circirt below:
2.It was similarly as above. When I used IO to enable the LDO,the IO couldn't be low without power,its power was about 1.2V.Cirecuit as below.
The structure of EN as below as similar as ADC:
My question is:
Why do IOs leakage electric?
Thanks!
Qianbo