Part Number: MSP430F155
Other Parts Discussed in Thread: MSP430FR2355
I need to implement high order Bessel filter with least delay and phase shift of the input signal. Output has to be filtered version of the input. Input is 50Khz samples of 420 Hz signal. Essentially the idea is to recover the 420 Hz tone from the samples without any substantial phase shift.So if the cut-off freq of a 10th order Bessel is approx 5 Khz, I suspect phase shift on 420 Hz will be < deg or so. You would think so?
Output also has to be "real time" meaning least delay.
Can this be implemented by using WDSP filter design techniques?
Then I need a DAC in the MCU.
I only find MSP430F155IPM, an LPQF 64 leadless device.
Isn't there a smaller device with DAC & with gull wing pins? As you see, I do not strictly need an ADC.
This will go in a miniature product with lots of such capabilities. So a small device will suffice.
Any help in selecting the right device will be appreciated.