This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F477: About current consumption of SD16

Part Number: MSP430F477


Hi community member!

I want to know current consumption of SD16 without internal reference voltage.

I’m looking at MSP430F477 datasheet of SD16_A, power supply and recommended opeating conditions and reference output buffer.

I think that one of the following two is correct.
Please tell me which is correct.
If they are both wrong, please tell me the correct answer.

I(SD16) : Analog supply current including internal reference(Datasheet P.42)
I(LOAD,Max) : Maximum load current on VREF(Datasheet P.45)

  • I(SD16) is including I(LOAD,Max). So current consumption of SD16 without internal reference voltage is (I(SD16) - I(LOAD,Max)). 
  • I(SD16) is not including current consumption of Maximum load current on VREF.

Best regards,
Cruijff

**Attention** This is a public forum