Part Number: MSP430F5659
Other Parts Discussed in Thread: MSP430F5529
Hi all,
I am connected a switch (on/off switch) with a custom board board of MSP430F5659. The interrupt configured for this is in HIGH_TO_LOW transition,
But interrupt takes place int both edges. The scenario is like when the switch is on one interrupt generated, when the switch turned off there also a interrupt generated.
What may be the reason for that, Kindly Help
Attaching my code
int main(void)
{
//clock() 8MHz
GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P4,GPIO_PIN4);
GPIO_enableInterrupt(GPIO_PORT_P4,GPIO_PIN4);
GPIO_selectInterruptEdge(GPIO_PORT_P4,GPIO_PIN4,GPIO_HIGH_TO_LOW_TRANSITION);
GPIO_clearInterrupt(GPIO_PORT_P4,GPIO_PIN4);
while(1)
{
}
}
#pragma vector=PORT4_VECTOR
__interrupt void Port_4(void)
{
case P4IV_P4IFG4:
if (P4IES & BIT4)
{
//interrupt generated
GPIO_clearInterrupt(GPIO_PORT_P4,GPIO_PIN4);
}
break;
}
Regards,
Renjith