This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR4133: External Sensor MCP9808 interfacing with MSP430FR4133

Part Number: MSP430FR4133
Other Parts Discussed in Thread: MSP430FR2100

Tool/software: IAR Embedded

 Hello,

 I'm a beginner on MSP430 and programming, and need some help with a project of mine.

Project- To interface an external temperature sensor MCP9808 through I2C communication with MSP430FR4133 to get temperature value.

Connections

SDA- pin 5.2

SCL- pin 5.3

GND-GND

VDD- 3.3V

I have interfaced a temperature sensor  MCP9808 with MSP430FR4133 through i2c communication. I am using the following code to read the temperature value from the sensor. I couldn't find the required results to get temperature value.

I am facing problem to get the desired results.

In MCP9808 data sheet in CONFIG Register part where I have to write

Addressbyte(0x30),Configuration pointer (0x01), MSB(0x00), LSB (0x08)

and read out Addressbyte(0x31), (0x00), (0x08) as a desired result but I am reading out Addressbyte(0x31), (0x00), (0x18), (0x01).

I have attached results below which are taken by logic analyzer. Any guidance to help me understand where I am doing mistake will be appreciated.

#define I2C__MSP430FR4133_H_

#include <MSP430.h>
#include <stdint.h>
#include <stdio.h>
#include <string.h>
#include "usci.h"

#define AMBIENT_TEMPERATURE		0x05
//#define Configuration_Reg		0x01
#define DEVICE_ID_REGISTER  		0x04
#define MANUFACTURE_ID_REGISTER	        0x0054
//#define AdressByte         	        0x30


 uint16_t tlen = 0;
 uint16_t rlen = 0;
 int *tx = NULL;
 int *rx = NULL;
 uint8_t addr = 0x18;
// void *tx =(void *)0x01;
// void *rx =(void *)0x00;

 
 
volatile unsigned char RXData;
volatile unsigned char TXData;

long Temperature;
void Stop_WD (void);
uint16_t I2C_TempRead(void);
uint16_t I2C_readMode(void);
void delay_tick(uint16_t);


unsigned char Adressbyte[10]; 
unsigned char Transmit [10]; 
unsigned char Meas_Receive [10];


int main(void)
{
 
  Stop_WD();
    
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5; 
Set_I2C();
//Transmit [0] =0x30 & 0xFE;
Transmit [0] = 0x01;
Transmit [1] = 0x00;
Transmit [2]=  0x08;

Meas_Receive [0] = 0x07;


__bis_SR_register(GIE);

I2C_write(&Transmit[0],3,addr);

delay_tick(500);

Set_I2C();

I2C_write_read (&Transmit[0],1,&Meas_Receive [0],3,addr);
//I2C_write(&Transmit[0],1,addr);
//I2C_read(&Meas_Receive [0],2,addr);

//I2C_readMode();
//I2C_TempRead();
//      
    while (1)
    {
        __delay_cycles(2000);
        while (UCB0CTL1 & UCTXSTP);         // Ensure stop condition got sent
        UCB0CTL1 |= UCTXSTT;                // I2C start condition
      
        __bis_SR_register(LPM0_bits|GIE);   // Enter LPM0 w/ interrupt
    }
}



#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = USCI_B0_VECTOR
__interrupt void USCIB0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_B0_VECTOR))) USCIB0_ISR (void)
#else
#error Compiler not supported!
#endif
{
  switch(__even_in_range(UCB0IV, USCI_I2C_UCBIT9IFG))
  {
    case USCI_NONE:          break;         // Vector 0: No interrupts
    case USCI_I2C_UCALIFG:   break;         // Vector 2: ALIFG
    case USCI_I2C_UCNACKIFG:                // Vector 4: NACKIFG
      UCB0CTL1 |= UCTXSTT;                  // resend start I2C start condition
      break;
    case USCI_I2C_UCSTTIFG:  break;         // Vector 6: STTIFG
    case USCI_I2C_UCSTPIFG:          // Vector 8: STPIFG
     TXData = 0;
     UCB0IFG &= ~UCSTPIFG;                 // Clear stop condition int flag
     break;
    case USCI_I2C_UCRXIFG3:  break;         // Vector 10: RXIFG3
    case USCI_I2C_UCTXIFG3:  break;         // Vector 14: TXIFG3
    case USCI_I2C_UCRXIFG2:  break;         // Vector 16: RXIFG2
    case USCI_I2C_UCTXIFG2:  break;         // Vector 18: TXIFG2
    case USCI_I2C_UCRXIFG1:  break;         // Vector 20: RXIFG1
    case USCI_I2C_UCTXIFG1:           // Vector 22: TXIFG1
//      UCB0TXBUF = TXData++;
      break; 
    case USCI_I2C_UCRXIFG0:                 // Vector 24: RXIFG0
      RXData = UCB0RXBUF;                   // Get RX data
      __bic_SR_register_on_exit(LPM0_bits); // Exit LPM0
      break;
    case USCI_I2C_UCTXIFG0:  break;         // Vector 26: TXIFG0
    case USCI_I2C_UCBCNTIFG: break;         // Vector 28: BCNTIFG
    case USCI_I2C_UCCLTOIFG: break;         // Vector 30: clock low timeout
    case USCI_I2C_UCBIT9IFG: break;         // Vector 32: 9th bit
    default: break;
  }
}

void Stop_WD (void)
 {
   WDTCTL = WDTPW | WDTHOLD;                                    // Stop WDT
 }
//
//
//void Device_ID(uint8_t device_reg)
//{
// 
//}
//
//void Manufacture_ID(uint8_t manufacture_reg)
//{
//  
//}
//
//void Ambient_Temp(uint8_t ambient_temp_reg)
//{
//  
//}                                                                                                                                                                            



uint16_t I2C_readMode(void)
{
  uint8_t UpperByte = 0;
  uint8_t LowerByte = 0;
  uint16_t data = 0;
  
//  UpperByte = i2c_read(); // READ 8 bits
////and Send ACK bit
//LowerByte = i2c_read(); // READ 8 bits
////and Send NAK bit
  
 data = UpperByte<<8|LowerByte;
 return data;
}

uint16_t I2C_TempRead(void)
{
 uint8_t UpperByte = 0; 
 uint8_t LowerByte = 0;
 uint16_t Temperature = 0;
 
 
 //Convert the temperature data
//First Check flag bits
if ((UpperByte & 0x80) == 0x80)
{                                                       //TA ³ TCRIT
}
if ((UpperByte & 0x40) == 0x40)
{                                                       //TA > TUPPER
}
if ((UpperByte & 0x20) == 0x20)
{                                                       //TA < TLOWER
}
UpperByte = UpperByte & 0x1F;                           //Clear flag bits

if ((UpperByte & 0x10) == 0x10)
{                                                       //TA < 0°C
UpperByte = UpperByte & 0x0F;                           //Clear SIGN
Temperature = 256 - (UpperByte * 16 + LowerByte / 16);
}
else 
{                                                       //TA ³ 0°C
Temperature = (UpperByte * 16 + LowerByte / 16);
                                                        //Temperature = Ambient Temperature (°C)
}
return Temperature;
}

void delay_tick(uint16_t tick)
{
  for (uint16_t i=0;i<tick; i++);
}


//----------------------------------------------I2C--------------------------------//

void Set_I2C(void)
{
  P5SEL0 |= BIT2 | BIT3;                  // I2C pins
 // Configure USCI_B0 for I2C mode 
  UCB0CTLW0 |= UCSWRST;                   // Software reset enabled
  UCB0CTLW0 |= UCMODE_3 | UCMST | UCSYNC; // I2C mode, Master mode, sync
  UCB0CTLW1 |= UCASTP_2;                  // Automatic stop generated

  UCB0BRW = 0x0008;                         // baudrate = SMCLK / 8
  UCB0TBCNT = 0x07;                       // number of bytes to be received
  UCB0I2CSA = 0x18;                       // Slave address is 0x18
  UCB0CTL1 &= ~UCSWRST;
  UCB0IE |= UCRXIE | UCNACKIE | UCBCNTIE ;
  
  
}



//------------------I2C_Master_write-------------------------------------------------//

uint32_t I2C_write(unsigned char* tx, uint32_t tlen,uint8_t addr)

{
  uint32_t r_val = 0;
  
  UCB0I2CSA = addr;                             // Assing slave address
  
  while ((UCB0IFG & UCSTPIFG));                 // Check if Stop condition on
  UCB0CTL1 |= UCTR + UCTXSTT;                   // Start writing through I2C
  while (!(UCB0IFG & UCTXIFG));                 // Wait until TX buffer ready
  for(uint32_t i = 0; i < tlen; i++) 
  {           
    UCB0TXBUF = *((uint8_t*)tx + i);            // Write string in  TX buffer of I2C        
    while (!(UCB0IFG & UCTXIFG));               // Wait until TX buffer ready
    if( i == tlen - 1) 
    {                                           // If only one byte left to write
      UCB0CTL1 |= UCTXSTP;                      // I2C stop condition
      UCB0IFG &= ~UCTXIFG;                      // Clear USCI_B0 TX int flag
    }
    r_val++;                                    // Increment return value
  }

  return r_val;
}

//----------------I2C_MASTER_READ--------------------------------------------------------//

uint32_t I2C_read(unsigned char* rx, uint32_t rlen, uint8_t addr)

{
  UCB0IFG &= ~UCSTPIFG;
  uint32_t r_val = 0;
  
  UCB0I2CSA = addr;                               // Assing slave address
  if (rlen != 0)
  {
    while ((UCB0CTL1 & UCTXSTP));                 // Check if Stop condition on
    UCB0CTL1 &= ~UCTR;                            // Set writing bit in register to 0
    UCB0CTL1 |= UCTXSTT;                          // Start reading through I2C
    while (!(UCB0CTL1 & UCTXSTT));                // start condition is not sent
    // only one byte
    if (rlen == 1)
    {
      while (!(UCB0IFG & UCRXIFG))                // wait until start condition is sent
      {
        if((UCB0CTL1 & UCTXSTT)==0)
          UCB0CTL1 |= UCTXSTP;                    // generate stop condition
      }
      while (UCB0CTL1 & UCTXSTP);                 // Ensure stop condition got sent
      *((uint8_t*)rx) = UCB0RXBUF;
      return 1;
    }
    // multiple bytes
    for (uint8_t i = 0; i < rlen-1; i++)
    {
      while (!(UCB0IFG & UCRXIFG));                // Wait until new data was written into RX buffer
      *((uint8_t*)rx + i) = UCB0RXBUF;              // Read RX buffer
      r_val ++;                                     // Increment return value      
    }
    UCB0CTL1 |= UCTXSTP;                            // Generate Stop condition  
    while (UCB0CTL1 & UCTXSTP);                     // Wait untill its generated
    *((uint8_t*)rx+rlen-1) = UCB0RXBUF;             // Read last byte 
  }
  return r_val++;
}

/*******************/

uint32_t I2C_write_read (unsigned char* tx,uint32_t tlen,unsigned char* rx, uint32_t rlen,uint8_t addr)
{
  
  uint32_t r_val = 0;
  
  UCB0I2CSA = addr;                             // Assing slave address
  
  while ((UCB0IFG & UCSTPIFG));                 // Check if Stop condition on
  UCB0CTL1 |= UCTR + UCTXSTT;                   // Start writing through I2C
  while (!(UCB0IFG & UCTXIFG));                 // Wait until TX buffer ready
  for(uint32_t i = 0; i < tlen; i++) 
  {           
    UCB0TXBUF = *((uint8_t*)tx + i);            // Write string in  TX buffer of I2C        
    while (!(UCB0IFG & UCTXIFG));               // Wait until TX buffer ready
    if( i == tlen - 1) 
    {                                           // If only one byte left to write
      UCB0CTL1 |= UCTXSTP;                      // I2C stop condition
      UCB0IFG &= ~UCTXIFG;                      // Clear USCI_B0 TX int flag
    }
    r_val++;                                    // Increment return value
  }
  
r_val = 0;
  
  if (rlen != 0)
  {
    while ((UCB0CTL1 & UCTXSTP));                 // Check if Stop condition on
    UCB0CTL1 &= ~UCTR;                            // Set writing bit in register to 0
    UCB0CTL1 |= UCTXSTT;                          // Start reading through I2C
    while (!(UCB0CTL1 & UCTXSTT));                // start condition is not sent
    // only one byte
    if (rlen == 1)
    {
      while (!(UCB0IFG & UCRXIFG))                // wait until start condition is sent
      {
        if((UCB0CTL1 & UCTXSTT)==0)
          UCB0CTL1 |= UCTXSTP;                    // generate stop condition
      }
      while (UCB0CTL1 & UCTXSTP);                 // Ensure stop condition got sent
      *((uint8_t*)rx) = UCB0RXBUF;
      return 1;
    }
    // multiple bytes
    for (uint8_t i = 0; i < rlen-1; i++)
    {
      while (!(UCB0IFG & UCRXIFG));                // Wait until new data was written into RX buffer
      *((uint8_t*)rx + i) = UCB0RXBUF;              // Read RX buffer
      r_val ++;                                     // Increment return value      
    }
    UCB0CTL1 |= UCTXSTP;                            // Generate Stop condition  
    while (UCB0CTL1 & UCTXSTP);                     // Wait untill its generated
    *((uint8_t*)rx+rlen-1) = UCB0RXBUF;             // Read last byte 
  }
  
  return r_val++; 
}

Thank you!

Mr. Shetty

Student

  • Hello Mr. Shetty,
    please let me first double check, whether I have understood the data you have provided correctly.
    So my understanding of the plots is, the first one is showing, what you're transmitting to the MCP device, what's according to your post matching what's written in the MCP datasheet.
    The second plot is showing in the second data block the response from the MCP device, which according to you should be (0x31), (0x00), (0x08) but in reality is (0x31) (0x00) (0x18) (0x01) (0xFF) (0xFF) according to the logic analyzer shots and that's also what you see on the MSP430 side.
    Is this a correct understanding?

    Best regards
    Peter
  • Hello Peter,

    Yes, you have understood correctly .

    Best Regards,
    Rajat Shetty
  • Hello Mr. Shetty,
    in this case this good and bad news.
    The good news is, this means the MSP430 I2C is transmitting and receiving what it should, means the MSP430 I2C is working correctly, but the Microchip device is not responding as it should.

    In this case I have two comments:
    1. If the MCP9808 means Microchip device is not responding as you expect, you need to get support from Microchip on this.
    2. Of course I have taken a glance on what the MCP9808 is about, finding out it is a temperature sensor. Looking at the pricing at a distributor it was for 1 one sample 1EUR. Now I am not sure whether you're aware, that all our MSP430 device equipped with an ADC do support temperature measurement with an integrated temperature sensor, including calibration values from factory for it in either the FLASH or FRAM memory. On one hand, this is the case with the MSP430FR4133 and its ADC, but even if you say, you need the temperature sensing device placed remotely, an MSP430FR2100 e.g. could do the job and costs at 1 sample about the half of the Microchip device.

    So maybe you should reconsider the whole thing.

    Once you hit MSP430 related issues, you can of course return back to us for support any time. Many thanks for your understanding.

    Best regards
    Peter
  • Hello Peter,

    Thanks for your response.

    Best Regards,

    Rajat Shetty

**Attention** This is a public forum