This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430G2553: Dispersion between MSP430G2553 units in capacitance measurement

Part Number: MSP430G2553
Other Parts Discussed in Thread: MSP430FR2512

Tool/software: Code Composer Studio

HI.
I am using an MSP430G2553, for a capacitive sensor that measures up to 200pf, with the Pin Oscillator method, shown in figure 8.1 of document SLAU144J. I use the Pinosc_01 example of MSP430Ware
Try a microcontroller with the pcb, and in the tests everything worked fine.
When I test several microcontrollers, an operating dispersion appears, more in the average measurement area than in the extremes, it reaches 3% and I need to reduce it to 1%.
I will try adding a crystal, and varying the timings so that the measurement value is as high as possible.
Any other idea? Maybe some other newer micro with Captivate technology is better?

**Attention** This is a public forum