Other Parts Discussed in Thread: MSP430F5502, MSP430WARE
Tool/software: TI C/C++ Compiler
When compiling code using the driverlib I am receiving a bunch of warnings like:
"C:/ti/ccs820/ccsv8/ccs_base/msp430/include/msp430f5xx_6xxgeneric.h", line 10207: warning #48-D: incompatible redefinition of macro "WDT_MDLY_8" (declared at line 4759 of "C:\ti\ccs820\ccsv8\ccs_base\msp430\include\msp430f5529.h")
It looks like the generic.h header is redefining a bunch of macros that are already defined in the msp430f5529.h header file. It appears that that both of these files are included in the hw_memmap.h file that is in driverlib.
Is there a good way to remove these warnings or a set of header files that do not cause these conflicts?
Thanks,
Kevin