Part Number: MSP430FR5969
Tool/software: Code Composer Studio
hi this is harikrishna...
Now i am working with SPI Protocols, my Question is like in MSP430FR596 P1.6, P1.5 are MOSI MISO..Now in Design two slaves one is Flash memory and another one is accelerometer both are working with SPI communication.. MISO and MOSI lines of both Slaves are connected to Single MISO ,MOSI of MSP internally..when i want to communicate with any of the slave I am making CHIP_SELECT pin as LOW so that i am working both Slaves one after one...the Problem is like if i write the data into flash memory continuously for 30 seconds in between this time Accelerometer motion will detect then what will happened.....i lost my writing data to the Flash ? or Motion will not work?....
thanks..